SFFS083 June 2021 TLIN2022A-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the TLIN2022A-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality |
| B | No device damage, but loss of functionality |
| C | No device damage, but performance degradation |
| D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the device pin diagram. For a detailed description of the device pins, please refer to the Pin Configuration and Functions section in the TLIN2022A-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| RXD1 | 1 | RXD1 biased dominant, no communication from LIN1 bus to MCU possible. | B |
| EN1 | 2 | LIN1 channel may only operate in standby mode after power on. If short on EN1 occurs in normal mode, LIN1 channel would be forced to enter sleep mode and could disable LIN communication. | B |
| TXD1 | 3 | TXD1 biased dominant, no communication from MCU to LIN1 bus possible. | B |
| RXD2 | 4 | RXD2 biased dominant, no communication from LIN2 bus to MCU possible. | B |
| EN2 | 5 | LIN2 channel may only operate in standby mode after power on. If short on EN2 occurs in normal mode, LIN2 channel would be forced to enter sleep mode and could disable LIN communication. | B |
| NC | 6 | No impact to performance. | D |
| TXD2 | 7 | TXD2 biased dominant, no communication from MCU to LIN2 bus possible. | B |
| GND | 8 | None | D |
| LIN2 | 9 | LIN2 biased dominant, no LIN communication possible. | B |
| VSUP | 10 | Device is unpowered and will not function. | B |
| NC | 11 | No impact to performance. | D |
| NC | 12 | No impact to performance. | D |
| LIN1 | 13 | LIN1 biased dominant, no LIN1 communication possible. | B |
| NC | 14 | No impact to performance. | D |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| RXD1 | 1 | No communication from LIN1 bus to MCU possible. | B |
| EN1 | 2 | Biased low due to internal pull-down so LIN1 in standby mode. | B |
| TXD1 | 3 | No communication from MCU to LIN1 bus possible. | B |
| RXD2 | 4 | No communication from LIN2 bus to MCU possible. | B |
| EN2 | 5 | Biased low due to internal pull-down so LIN2 in standby mode. | B |
| NC | 6 | No impact to performance. | D |
| TXD2 | 7 | No communication from MCU to LIN2 bus possible. | B |
| GND | 8 | Device is unpowered and will not function. | B |
| LIN2 | 9 | No LIN2 communication possible. | B |
| VSUP | 10 | Device is unpowered and will not function. | B |
| NC | 11 | No impact to performance. | D |
| NC | 12 | No impact to performance. | D |
| LIN1 | 13 | No LIN1 communication possible. | B |
| NC | 14 | No impact to performance. | D |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| RXD1 | 1 | EN1 | LIN1 will go into sleep mode when a dominant bit is received on the LIN1 bus, disabling communication. | B |
| EN1 | 2 | TXD1 | With TXD toggling, LIN1 channel will transition between normal and sleep mode, corrupting communication. | B |
| TXD1 | 3 | RXD2 | Communication on TXD1 will corrupt the received data from LIN2 to RXD2. | B |
| RXD2 | 4 | EN2 | With data toggling on RXD2 via LIN2 bus, EN2 toggles and causes LIN2 channel to transition between normal and sleep modes. | B |
| EN2 | 6 | NC | No impact to performance. | D |
| NC | 7 | TXD2 | No impact to performance. | D |
| GND2 | 8 | LIN2 | LIN2 biased dominant, no LIN1 communication possible. | B |
| LIN2 | 9 | VSUP | LIN2 biased recessive, no LIN2 communication possible. | B |
| VSUP | 10 | NC | No impact to performance. | D |
| NC | 11 | NC | No impact to performance. | D |
| NC | 12 | LIN1 | No impact to performance. | D |
| LIN1 | 13 | NC | No impact to performance. | D |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| RXD1 | 1 | Absolute maximum voltage violation, transceiver may be damaged. | A |
| EN1 | 2 | Absolute maximum voltage violation, transceiver may be damaged. | A |
| TXD1 | 3 | Absolute maximum voltage violation, transceiver may be damaged. | A |
| RXD2 | 4 | Absolute maximum voltage violation, transceiver may be damaged. | A |
| EN2 | 5 | Absolute maximum voltage violation, transceiver may be damaged. | A |
| NC | 6 | No impact to performance. | D |
| TXD2 | 7 | Absolute maximum voltage violation, transceiver may be damaged. | A |
| GND | 8 | Device is unpowered and will not function. | B |
| LIN2 | 9 | LIN2 biased recessive, no LIN2 communication possible. | B |
| VSUP | 10 | None | D |
| NC | 11 | No impact to performance. | D |
| NC | 12 | No impact to performance. | D |
| LIN1 | 13 | LIN1 biased recessive, no LIN1 communication possible. | B |
| NC | 14 | No impact to performance. | D |