SDAA391 June 2026 TPS922050 , TPS922051 , TPS922052 , TPS922053 , TPS922054 , TPS922055
Reducing shifts the dominant compensation pole to a higher frequency and increases the loop gain in the low-to-mid-frequency range. As a result, the current regulation loop can achieve a higher crossover frequency and a faster transient response, provided that sufficient phase margin is maintained. Figure 3-2 and Table 3-1 show the simulation results. During PWM dimming turn-on, this faster response helps the LED current reach its target value more quickly, thereby reducing the LED-current rising time. However, a smaller may increase the overshoot of LED current. Therefore, should be selected by balancing dimming response speed, loop stability, peak LED current.
Figure 3-2 Loop Simulation with Different
CCOMP| (pF) | Peak Current (A) | Rising Time (us) |
|---|---|---|
| 470 | 3.81 | 4.21 |
| 690 | 3.61 | 4.36 |
| 910 | 3.42 | 4.92 |
| 1000 | 3.29 | 6.11 |