To set up the GUI the first time:
- Make sure that the previously mentioned driver is installed successfully so that everything works properly and that the GUI can update the EVM firmware, if necessary.
- Check to make sure the EVM and SCB Controller unit
is plugged into the PC, then go to the previously-provided GUI link.
- Verify that the EVM is connected to the SCB before
plugging the SCB into a USB port.
- Open the GUI Composer application to launch the GUI from the web browser (see Figure 3-2).
- The GUI link brings up all versions of the GUI. TI recommends launching the newest version available.
- For first-time GUI Composer setup, follow the prompts to download the TI Cloud Agent and browser extension (see Figure 3-3). These prompts appear after closing the README.md dialog box.
- Optionally, to download the GUI for offline use,
select the
icon in the GUI Composer application and
follow the prompts (see Figure 3-2).