SBOU244 June   2020 INA281

 

  1.   INA281EVM
    1.     Trademarks
    2. 1 General Texas Instruments High Voltage Evaluation (TI HV EVM) User Safety Guidelines
    3. 2 Overview
      1. 2.1 EVM Kit Contents
      2. 2.2 Related Documentation From Texas Instruments
    4. 3 Hardware
      1. 3.1 Features
    5. 4 Operation
      1. 4.1 Quick Start Setup
      2. 4.2 Measurements
    6. 5 EVM Components
      1. 5.1 R2_Xn, R3_Xn, R4_Xn, C2_Xn, C3_Xn
      2. 5.2 C1_Xn
      3. 5.3 R1_Xn
      4. 5.4 U1_Xn (INA281)
    7. 6 Schematic, PCB Layout, and Bill of Materials
      1. 6.1 Schematics
      2. 6.2 PCB Layout
      3. 6.3 Bill of Materials
        1. 6.3.1 Bill of Materials

U1_Xn (INA281)

U1_Xn is the location for the INA281Xn test device.

The following list of factors are involved in selecting the appropriate device gain:

  • The differential input voltage is either applied across the inputs or developed based on the load current that flows through the shunt resistor.
  • Make sure that the output voltage does not exceed the supply voltage. This limiting factor requires attention to device selection.
  • The selected device must allow the output voltage to remain within the acceptable range after the developed input voltage is amplified by the respective device gain. The output voltage must remain within the device-specified swing limitations for response in the linear range.
  • An output below the minimum allowable output requires the selection of a device with a higher gain. Likewise, an output above the maximum allowable output requires the selection of a device with a lower gain.