SBOK083A August   2024  – October 2024 TMUX582F-SEP

 

  1.   1
  2.   2
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 Single-Event Latch-Up (SEL) Results
    2. 5.2 Event Rate Calculations
    3. 5.3 Single-Event Transients (SET) Results
  9. 6Summary
  10. 7References
  11. 8Revision History

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by the TAMU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For this study, ion flux of 105 ions / cm2 * s were used to provide heavy-ion fluences of approximately 107 ions / cm2 for SEL testing and ion flux of 104 ions / cm2 * s were used to provide heavy-ion fluences of approximately 106 ions / cm2 for SET testing.

For the experiments conducted on this report, 109Ag ions at angle of incidence of 0° for an LETEFF of 43MeV × cm2 / mg were used. The total kinetic energy of 109Ag in the vacuum is 1.634GeV (15 MeV/nucleon). Ion uniformity for these experiments was between 93% and 97%.

Figure 4-1 shows one of the TMUX582F-SEP test boards used for experiments at the TAMU Cyclotron Radiation Effects Facility. The in-air gap between the device and the ion beam port window was maintained at 40mm for all runs.

TMUX582F-SEP TMUX582F-SEP Evaluation Board at the TAMU Cyclotron Radiation Effects FacilityFigure 4-1 TMUX582F-SEP Evaluation Board at the TAMU Cyclotron Radiation Effects Facility