SCDS219B NOVEMBER   2005  – May 2015 TS5A3157

PRODUCTION DATA.  

  1. Features
  2. Applications
  3. Description
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
    5. 6.5 Electrical Characteristics for 5-V Supply
    6. 6.6 Electrical Characteristics for 3.3-V Supply
    7. 6.7 Electrical Characteristics for 2.5-V Supply
    8. 6.8 Electrical Characteristics for 1.8-V Supply
    9. 6.9 Typical Characteristics
  7. Parameter Measurement Information
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
      3. 9.2.3 Application Curve
  10. 10Power Supply Recommendations
  11. 11Layout
    1. 11.1 Layout Guidelines
    2. 11.2 Layout Example
  12. 12Device and Documentation Support
    1. 12.1 Device Support
      1. 12.1.1 Device Nomenclature
    2. 12.2 Documentation Support
      1. 12.2.1 Related Documentation
    3. 12.3 Community Resources
    4. 12.4 Trademarks
    5. 12.5 Electrostatic Discharge Caution
    6. 12.6 Glossary
  13. 13Mechanical, Packaging, and Orderable Information

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

12 Device and Documentation Support

12.1 Device Support

12.1.1 Device Nomenclature

Table 2. Parameter Description

SYMBOL DESCRIPTION
VCOM Voltage at COM
VNC Voltage at NC
VNO Voltage at NO
ron Resistance between COM and NC or COM and NO ports when the channel is ON
Δron Difference of ron between channels in a specific device
ron(flat) Difference between the maximum and minimum value of ron in a channel over the specified range of conditions
INC(OFF) Leakage current measured at the NC port, with the corresponding channel (NC to COM) in the OFF state
INO(OFF) Leakage current measured at the NO port, with the corresponding channel (NO to COM) in the OFF state
INC(ON) Leakage current measured at the NC port, with the corresponding channel (NC to COM) in the ON state and the output (COM) open
INO(ON) Leakage current measured at the NO port, with the corresponding channel (NO to COM) in the ON state and the output (COM) open
ICOM(ON) Leakage current measured at the COM port, with the corresponding channel (COM to NO or COM to NC) in the ON state and the output (NC or NO) open
VIH Minimum input voltage for logic high for the control input (IN)
VIL Maximum input voltage for logic low for the control input (IN)
VI Voltage at the control input (IN)
IIH, IIL Leakage current measured at the control input (IN)
tON Turn-on time for the switch. This parameter is measured under the specified range of conditions and by the propagation delay between the digital control (IN) signal and analog output (COM, NC, or NO) signal when the switch is turning ON.
tOFF Turn-off time for the switch. This parameter is measured under the specified range of conditions and by the propagation delay between the digital control (IN) signal and analog output (COM, NC, or NO) signal when the switch is turning OFF.
tBBM Break-before-make time. This parameter is measured under the specified range of conditions and by the propagation delay between the output of two adjacent analog channels (NC and NO) when the control signal changes state.
QC Charge injection is a measurement of unwanted signal coupling from the control (IN) input to the analog (NC, NO, or COM) output. This is measured in coulomb (C) and measured by the total charge induced due to switching of the control input. Charge injection, QC = CL  × ΔVCOM, CL is the load capacitance and ΔVCOM is the change in analog output voltage.
CNC(OFF) Capacitance at the NC port when the corresponding channel (NC to COM) is OFF
CNO(OFF) Capacitance at the NO port when the corresponding channel (NO to COM) is OFF
CNC(ON) Capacitance at the NC port when the corresponding channel (NC to COM) is ON
CNO(ON) Capacitance at the NO port when the corresponding channel (NO to COM) is ON
CCOM(ON) Capacitance at the COM port when the corresponding channel (COM to NC or COM to NO) is ON
CI Capacitance of control input (IN)
OISO OFF isolation of the switch is a measurement of OFF-state switch impedance. This is measured in dB in a specific frequency, with the corresponding channel (NC to COM or NO to COM) in the OFF state.
XTALK Crosstalk is a measurement of unwanted signal coupling from an ON channel to an OFF channel (NC to NO or NO to NC). This is measured in a specific frequency and in dB.
BW Bandwidth of the switch. This is the frequency where the gain of an ON channel is –3 dB below the DC gain.
THD Total harmonic distortion describes the signal distortion caused by the analog switch. This is defined as the ratio of root mean square (RMS) value of the second, third, and higher harmonic to the absolute magnitude of fundamental harmonic.
I+ Static power-supply current with the control (IN) pin at V+ or GND

12.2 Documentation Support

12.2.1 Related Documentation

For related documentation, see the following:

  • Implications of Slow or Floating CMOS Inputs, SCBA004

12.3 Community Resources

The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.

    TI E2E™ Online Community TI's Engineer-to-Engineer (E2E) Community. Created to foster collaboration among engineers. At e2e.ti.com, you can ask questions, share knowledge, explore ideas and help solve problems with fellow engineers.
    Design Support TI's Design Support Quickly find helpful E2E forums along with design support tools and contact information for technical support.

12.4 Trademarks

E2E is a trademark of Texas Instruments.

All other trademarks are the property of their respective owners.

12.5 Electrostatic Discharge Caution

esds-image

These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.

12.6 Glossary

SLYZ022TI Glossary.

This glossary lists and explains terms, acronyms, and definitions.