ZHCSKD3A November 2019 – February 2021 TPS6521815
PRODUCTION DATA
In OFF mode, the PMIC is completely shut down with the exception of a few circuits to monitor the AC_DET, PWR_EN, and PB input. All power rails are turned off and the registers are reset to their default values. The I2C communication interface is turned off. This is the lowest-power mode of operation. To exit OFF mode VIN_BIAS must exceed the UVLO threshold and one of the following wake-up events must occur:
To enter the OFF state, ensure that all power rails are assigned to the sequencer, then pull the PWR_EN pin low. Additionally, if the OFFnPFO bit is set to 1b and the PFI input falls below the power fail threshold the device transitions to the OFF state. If the freshness seal is broken, DCDC5 and DCDC6 remains on in the OFF state. If a PGOOD or OTS fault occurs while in the ACTIVE state, TPS6521815 will transition to the RESET state.