SLDS153B May 2009 – November 2015 TMP815
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TMP815 device needs few external components for the features described in Feature Description . The device needs a 1-uF or greater capacitor connected at VCC. The device generates 5-V regulated output which can be used for pullups in the circuit as well as the Hall sensor.
Figure 5 shows the typical application diagram.
Figure 5. 12-V Sample Application Circuit
For this design example, use the following parameters:
Pins:
Power Supply:
Build the circuit with the recommended connections at the pins.
Test the motor circuit with hardware connected to it.
Figure 6. Start-up at 12 V (Soft Start)
Figure 8. Motor Outputs and Phase Current at Duty Cycle < 100%
Figure 7. Motor Outputs and Phase Current at 100% Duty Cycle
Figure 9. Motor Outputs and Phase Currents at 100% Duty Cycle and With Hall Sensor Data