ZHCSFK1D July 2016 – January 2025
PRODUCTION DATA
Ceramic, 1.0µF, X5R- and X7R-type capacitors are recommended because these capacitors have minimal variation in value and equivalent series resistance (ESR) over temperature.
However, the TLV700xx-Q1 devices are designed to be stable with an effective capacitance of 0.1µF or larger at the output. Thus, these devices are stable with capacitors of other dielectric types as well, as long as the effective capacitance under operating bias voltage and temperature is greater than 0.1µF. This effective capacitance refers to the capacitance under the operating bias voltage and temperature conditions; that is, the capacitance after taking both bias voltage and temperature derating into consideration. In addition to allowing the use of cheaper dielectrics, this capability of being stable with 0.1µF effective capacitances also enables the use of smaller-footprint capacitors that have higher derating in size- and space-constrained applications.
Note that using a 0.1µF rated capacitor at the output of the LDO does not provide stability because the effective capacitance under the specified operating conditions is less than 0.1µF. Maximum ESR must be less than 200mΩ.
Although an input capacitor is not required for stability, good analog design practice is to connect a 0.1µF to 1µF, low-ESR capacitor across the IN pin and the GND pin of the regulator. This capacitor counteracts reactive input sources and improves transient response, noise rejection, and ripple rejection. A higher-value capacitor may be necessary if large, fast, rise-time load transients are anticipated, or if the device is not located close to the power source. If source impedance is more than 2Ω, a 0.1µF input capacitor may be necessary to provide stability.