ZHCSMI4 november 2020 TAS6424MS-Q1
PRODUCTION DATA
The pinout of the TAS6424MS-Q1 was selected to provide flowthrough layout with all high-power connections on the right side, and all low-power signals and supply decoupling on the left side.
Figure 12-1 shows the area for the components in the application example (see the Typical Applications section).
The TAS6424MS-Q1 EVM uses a four-layer PCB. The copper thickness was selected as 70 µm to optimize power loss.
The small value of the output filter provides a small size and, in this case, the low height of the inductor enables double-sided mounting.
The EVM PCB shown in Figure 12-1 is the basis for the layout guidelines.