ZHCSK17AC March 1993 – April 2022 SN54LVC14A , SN74LVC14A
PRODUCTION DATA
请参考 PDF 数据表获取器件具体的封装图。
The signal effects of the debounce circuit can be seen when comparing Figure 9-2 and Figure 9-3. In Figure 9-2, the input is a very poor quality signal due to the error in the physical push button. If the MCU attempts to sample this input to detect a push, there is high probability that multiple push events will be falsely detected. Once the debounce circuit has been implemented, the input is cleaned up, and the MCU can perform push detection without any error, as seen in Figure 9-3.
Figure 9-1 Debouncer Application Diagram