ZHCSLM9A August 2020 – February 2021 LP8866S-Q1
PRODUCTION DATA
The LEDSET resistor missing or invalid is detected if the resistor is not assembled or not valid value as requested during the initialization. The LP8866S-Q1 device defaults to 6-channel/150-mA configuration if the LEDSET resistor is missing or invalid. The LEDSET_STATUS fault bit is set in the BOOST_FAULT_STATUS register. The LEDSET resistor missing or invalid fault will not be monitored after initialization, so that the LP8866S-Q1 is operating in the configuration determined during initialization even though the LEDSET resistor is missing or invalid after initialization.