SNVS416C November   2005  – February 2016 LM27951

PRODUCTION DATA.  

  1. 1 Features
  2. 2 Applications
  3. 3 Description
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
    6. 6.6 Typical Characteristics
  7. 7 Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Charge Pump
      2. 7.3.2 Soft Start
      3. 7.3.3 Thermal Protection
    4. 7.4 Device Functional Modes
      1. 7.4.1 Enable and PWM Pins
      2. 7.4.2 Adjusting LED Brightness (PWM Control)
  8. 8 Application and Implementation
    1. 8.1 Application Information
      1. 8.1.1 Maximum Output Current, Maximum LED Voltage, Minimum Input Voltage
    2. 8.2 Typical Application
      1. 8.2.1 Design Requirements
      2. 8.2.2 Detailed Design Procedure
        1. 8.2.2.1 Setting LED Currents
        2. 8.2.2.2 Capacitor Selection
        3. 8.2.2.3 Parallel Dx Outputs for Increased Current Drive
        4. 8.2.2.4 Power Efficiency
        5. 8.2.2.5 Power Dissipation
      3. 8.2.3 Application Curves
  9. 9 Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11Device and Documentation Support
    1. 11.1 Device Support
      1. 11.1.1 Third-Party Products Disclaimer
    2. 11.2 Documentation Support
      1. 11.2.1 Related Documentation
    3. 11.3 Community Resources
    4. 11.4 Trademarks
    5. 11.5 Electrostatic Discharge Caution
    6. 11.6 Glossary
  12. 12Mechanical, Packaging, and Orderable Information

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

8 Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

8.1 Application Information

8.1.1 Maximum Output Current, Maximum LED Voltage, Minimum Input Voltage

The LM27951 can drive 4 LEDs at 30 mA each from an input voltage as low as 3 V, so long as the LEDs have a forward voltage of 3.6 V or less (room temperature).

The previous statement is a simple example of the LED drive capabilities of the LM27951. The statement contains key application parameters required to validate an LED-drive design using the LM27951: LED current (ILED), number of active LEDs (N), LED forward voltage (VLED), and minimum input voltage (VIN-MIN).

Equation 1 can be used to estimate the total output current capability of the LM27951:

Equation 1. ILED_MAX = ((1.5 × VIN) – VLED) / ((N × ROUT) + kHR

where

  • ROUT = output resistance

As an example of Equation 1: ILED_MAX = ((1.5 × VIN ) – VLED) / ((N × 3.3 Ω) + 12 mV/mA).

This parameter models the internal losses of the charge pump that result in voltage droop at the pump output VOUT. Because the magnitude of the voltage droop is proportional to the total output current of the charge pump, the loss parameter is modeled as a resistance. The output resistance of the LM27951 is typically 3.3 Ω (VIN = 3 V, TA = 25°C – see Equation 2).

Equation 2. VVOUT = 1.5 × VIN – N × ILED × ROUT

where

  • kHR = headroom constant
  • ROUT = output resistance

This parameter models the minimum voltage required across the current sources for proper regulation. This minimum voltage is proportional to the programmed LED current, so the constant has units of mV/mA. The typical kHR of the LM27951 is 12 mV/mA – see Equation 3:

Equation 3. (VVOUT – VLED) > kHR × ILED

Maximum LED current is highly dependent on minimum input voltage and LED forward voltage. Output current capability can be increased by raising the minimum input voltage of the application, or by selecting LEDs with a lower forward voltage. Excessive power dissipation may also limit output current capability of an application.

8.2 Typical Application

LM27951 20171701.gif Figure 5. LM27951 Typical Application

8.2.1 Design Requirements

For typical white-LED switched capacitor applications, use the parameters listed in Table 1.

Table 1. Design Parameters

DESIGN PARAMETER EXAMPLE VALUE
Minimum input voltage 2.8 V
Output current 20 mA
RSET 12.5 kΩ

8.2.2 Detailed Design Procedure

8.2.2.1 Setting LED Currents

The current through the four LEDs connected to D1-4 can be set to a desired level simply by connecting an appropriately sized resistor (RSET) between the ISET pin of the LM27951 and GND. The LED currents are proportional to the current that flows out of the ISET pin and are a factor of 200 times greater than the ISET current. The feedback loop of an internal amplifier sets the voltage of the ISET pin to 1.25 V (typical). The previous statements are simplified in Equation 4 and Equation 5:

Equation 4. IDx = 200 × (VSET / RSET)
Equation 5. RSET = 200 × (1.25 V / IDx)

8.2.2.2 Capacitor Selection

The LM27951 requires 4 external capacitors for proper operation. Surface-mount multi-layer ceramic capacitors are recommended. These capacitors are small, inexpensive and have very low equivalent series resistance (ESR) — < 20 mΩ typical. Tantalum capacitors, OS-CON capacitors, and aluminum electrolytic capacitors are not recommended for use with the LM27951 due to their high ESR, compared to ceramic capacitors.

For most applications, it is preferable to use ceramic capacitors with X7R or X5R temperature characteristic with the LM27951. These capacitors have tight capacitance tolerance (as good as ±10%) and hold their value over temperature (X7R: ±15% over –55°C to 125°C; X5R: ±15% over –55°C to +85°C).

Capacitors with Y5V or Z5U temperature characteristic are generally not recommended for use with the LM27951. Capacitors with these temperature characteristics typically have wide capacitance tolerance (80%, –20%) and vary significantly over temperature (Y5V: 22%, –82% over –30°C to +85°C range; Z5U: 22%, –56% over 10°C to 85°C range). Under some conditions, a nominal 1-µF Y5V or Z5U capacitor could have a capacitance of only 0.1 µF. Such detrimental deviation is likely to cause Y5V and Z5U capacitors to fail to meet the minimum capacitance requirements of the LM27951.

The voltage rating of the output capacitor must be 10 V or more. All other capacitors must have a voltage rating at or above the maximum input voltage of the application.

8.2.2.3 Parallel Dx Outputs for Increased Current Drive

Outputs D1-4 may be connected together to drive a one or two LEDs at higher currents. In a one LED configuration, all four parallel current sources of equal value are connected together to drive a single LED. The LED current programmed must be chosen such that the current provided from each of the outputs is programmed to 25% of the total desired LED current. For example, if 60 mA is the desired drive current for the single LED, RSET must be selected so that the current out of each current source is 15 mA. Similarly, if two LEDs are to be driven by pairing up the D1-4 outputs (that is, D1-2, D3-4), RSET must be selected so that the current out of each current source output is 50% of the desired LED current.

Connecting the outputs in parallel does not affect the internal operation of the LM27951 and has no impact on the electrical characteristics and limits previously presented. The available diode output current, maximum diode voltage, and all other specifications provided in the Electrical Characteristics apply to this parallel output configuration, just as they do to the standard 4-LED application circuit.

8.2.2.4 Power Efficiency

Efficiency of LED drivers is commonly taken to be the ratio of power consumed by the LEDs (PLED) to the power drawn at the input of the part (PIN). With a 1.5×/1× charge pump, the input current is equal to the charge pump gain times the output current (total LED current). For a simple approximation, the current consumed by internal circuitry can be neglected and the efficiency of the LM27951 can be predicted as follows:

Equation 6. PLED = N × VLED × ILED
Equation 7. PIN = VIN × IIN
Equation 8. PIN = VIN × (Gain × N × ILED + IQ)
Equation 9. E = (PLED / PIN)

Neglecting IQ results in a slightly higher efficiency prediction, but this impact is no more than a few percentage points when several LEDs are driven at full power. It is also worth noting that efficiency as defined here is in part dependent on LED voltage. Variation in LED voltage does not affect power consumed by the circuit and typically does not relate to the brightness of the LED. For an advanced analysis, it is recommended that power consumed by the circuit (VIN × IIN) be evaluated rather than power efficiency.

8.2.2.5 Power Dissipation

The power dissipation (PDISSIPATION) and junction temperature (TJ) can be approximated with Equation 10 and Equation 11. PIN is the power generated by the 1.5×/1× charge pump, PLED is the power consumed by the LEDs, TAis the ambient temperature, and RθJA is the junction-to-ambient thermal resistance for the 14-pin WSON package. VIN is the input voltage to the LM27951, VLED is the nominal LED forward voltage, and ILED is the programmed LED current.

Equation 10. PDISSIPATION = PIN – PLED = [Gain × VIN × (4 x ILED)] − (VLED × 4 × ILED)
Equation 11. TJ = TA + (PDISSIPATION × RθJA)

The junction temperature rating takes precedence over the ambient temperature rating. The LM27951 may be operated outside the ambient temperature rating, so long as the junction temperature of the device does not exceed the maximum operating rating of 115°C. The maximum ambient temperature rating must be derated in applications where high power dissipation and/or poor thermal resistance causes the junction temperature to exceed 115°C.

8.2.3 Application Curves

LM27951 20171708.png
Figure 6. Converter Efficiency vs Input Voltage
LM27951 20171709.png
Figure 7. LED Current vs RSET