see (1) | MIN | MAX | UNIT |
|---|
| Supply voltage | VDD | Supply voltage for LVCMOS core logic(2) Supply voltage for LPSDR low speed interface | –0.5 | 2.3 | V |
| VDDI | Supply voltage for SubLVDS receivers(2) | –0.5 | 2.3 | V |
| VOFFSET | Supply voltage for HVCMOS and micromirror electrode(2) (3) | –0.5 | 11 | V |
| VBIAS | Supply voltage for micromirror electrode(2) | –0.5 | 19 | V |
| VRESET | Supply voltage for micromirror electrode(2) | –15 | 0.5 | V |
| | VDDI–VDD | | Supply voltage delta (absolute value)(4) | | 0.3 | V |
| | VBIAS–VOFFSET | | Supply voltage delta (absolute value)(5) | | 11 | V |
| | VBIAS–VRESET | | Supply voltage delta (absolute value)(6) | | 34 | V |
| Input voltage | Input voltage for other inputs LPSDR(2) | –0.5 | VDD + 0.5 | V |
| Input voltage for other inputs SubLVDS(2) (7) | –0.5 | VDDI + 0.5 | V |
| Input pins | | VID | | SubLVDS input differential voltage (absolute value)(7) | | 810 | mV |
| IID | SubLVDS input differential current | | 10 | mA |
| Clock frequency | ƒclock | Clock frequency for low speed interface LS_CLK | | 130 | MHz |
| ƒclock | Clock frequency for high speed interface DCLK | | 620 | MHz |
| Environmental | TARRAY and TWINDOW | Temperature – operational (8) | –20 | 90 | °C |
| Temperature – non-operational(8) | –40 | 90 | °C |
| TDP | Dew Point Temperature - operating and non-operating (non-condensing) | | 81 | °C |
| |TDELTA| | Absolute Temperature delta between any point on the window edge and the ceramic test point TP1(9) | | 30 | °C |
(1) Operation outside the Absolute Maximum Ratings may cause permanent device
damage. Absolute Maximum Ratings do not imply
functional operation of the device at these or any
other conditions beyond those listed under
Recommended Operating Conditions. If outside the
Recommended Operating Conditions but within the
Absolute Maximum Ratings, the device may not be
fully functional, and this may affect device
reliability, functionality, performance, and
shorten the device lifetime.
(2) All voltage values are with respect to the ground terminals (VSS). The following power supplies are all required to operate the DMD: VDD, VDDI, VOFFSET, VBIAS, and VRESET. All VSS connections are also required.
(3) VOFFSET supply transients must fall within specified voltages.
(4) Exceeding the recommended allowable absolute voltage difference between VDDI and VDD may result in excessive current draw.
(5) Exceeding the recommended allowable absolute voltage difference between VBIAS and VOFFSET may result in excessive current draw.
(6) Exceeding the recommended allowable absolute voltage difference between VBIAS and VRESET may result in excessive current draw.
(7) This maximum input voltage rating applies when each input of a differential pair is at the same voltage potential. Sub-LVDS differential inputs must not exceed the specified limit or damage may result to the internal termination resistors.
(8) The highest temperature of the active array (as calculated by the
Section 7.6) or of any point along the
Window Edge as defined in
Figure 7-1. The locations of thermal test
points TP2, TP3, TP4, and TP5 in
Figure 7-1 are intended to measure the
highest window edge temperature. If a particular
application causes another point on the window
edge to be at a higher temperature, that point
should be used.
(9) Temperature delta is the highest difference between the ceramic test point 1
(TP1) and anywhere on the window edge as shown in
Figure 7-1. The window test points TP2, TP3,
TP4, and TP5 shown in
Figure 7-1 are intended to result in the
worst case delta. If a particular application
causes another point on the window edge to result
in a larger delta temperature, that point should
be used.