| 15:9 |
Reserved |
RW |
0000000 |
Reserved |
| 8 |
VBGR_SLEEP |
RW |
0 |
Turns off the 'bandgap-over-R' bias |
| 7 |
Reserved |
RW |
0 |
Reserved |
| 6 |
TSENSE_SLEEP |
RW |
0 |
Turns off the temperature sensor |
| 5 |
PLL_SLEEP |
RW |
1 |
Puts the PLL into sleep mode (FUSE
Controlled) |
| 4 |
CLKRECV_SLEEP |
RW |
0 |
When asserted the clock input receiver gets put into
sleep mode. This also affects the FIFO_OSTR receiver as
well. |
| 3 |
DACA_SLEEP |
RW |
0 |
Puts the DACA into sleep mode |
| 2 |
DACB_SLEEP |
RW |
0 |
Puts the DACB into sleep mode |
| 1 |
CLK_TX_SLEEP |
RW |
1 |
When asserted the PLL TX clock output is in low power
mode. |
| 0 |
Reserved |
RW |
0 |
Reserved |