ZHCSJM7 April 2019 BQ79606A-Q1
PRODUCTION DATA.
The BQ79606A-Q1 always operates in one of four modes. The mode depends on the stack voltage and the operational requirements of the system. A high level description of the modes is as follows:
Figure 21 is a flow diagram of the transition between each of the modes. The modes are described in greater detail in the following sections.
Figure 21. Power States Flow