SLUS977B September   2009  – August 2015

PRODUCTION DATA.  

  1. 1 Features
  2. 2 Applications
  3. 3 Description
  4. 4 Revision History
  5. 5 Device Comparison Table
  6. 6 Pin Configuration and Functions
  7. 7 Specifications
    1. 7.1 Absolute Maximum Ratings
    2. 7.2 ESD Ratings
    3. 7.3 Recommended Operating Conditions
    4. 7.4 Thermal Information
    5. 7.5 Electrical Characteristics
    6. 7.6 Typical Characteristics
  8. 8 Detailed Description
    1. 8.1 Overview
    2. 8.2 Functional Block Diagram
    3. 8.3 Feature Description
      1. 8.3.1 Input Overvoltage Protection
      2. 8.3.2 Input Overcurrent Protection
      3. 8.3.3 Battery Overvoltage Protection
      4. 8.3.4 Thermal Protection
      5. 8.3.5 Enable Function
      6. 8.3.6 PGATE Output
    4. 8.4 Device Functional Modes
      1. 8.4.1 OPERATION Mode
      2. 8.4.2 POWER-DOWN Mode
      3. 8.4.3 POWER-ON RESET Mode
  9. 9 Application and Implementation
    1. 9.1 Application Information
    2. 9.2 Typical Application
      1. 9.2.1 Design Requirements
      2. 9.2.2 Detailed Design Procedure
        1. 9.2.2.1 Selection of RBAT
        2. 9.2.2.2 Selection of RCE
        3. 9.2.2.3 Selection of Input and Output Bypass Capacitors
        4. 9.2.2.4 Selection of the PGATE External MOSFET
      3. 9.2.3 Application Curves
  10. 10Power Supply Recommendations
  11. 11Layout
    1. 11.1 Layout Guidelines
    2. 11.2 Layout Example
  12. 12Device and Documentation Support
    1. 12.1 Community Resources
    2. 12.2 Trademarks
    3. 12.3 Electrostatic Discharge Caution
    4. 12.4 Glossary
  13. 13Mechanical, Packaging, and Orderable Information

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

9 Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

9.1 Application Information

The bq24308 device protects against overvoltage, overcurrent, and battery overvoltage events that occur due to faulty adapter or other input sources. If any of these faults occur, the bq24308 device isolates the downstream devices from the input source.

9.2 Typical Application

The typical values for an application are VOVP = 6.3 V, IOCP = 700 mA, and BVOVP = 4.35 V.

bq24308 typ_app_cir_lus977.gif
Terminal numbers shown are for the 2 × 2 DSG package.
Figure 11. Typical Application Diagram

9.2.1 Design Requirements

For this design example, use the parameters listed in Table 1.

Table 1. Design Parameters

DESIGN PARAMETER EXAMPLE VALUE
Supply Voltage 5 V
INILIM 1 A

9.2.2 Detailed Design Procedure

9.2.2.1 Selection of RBAT

It is strongly recommended that the battery not be tied directly to the VBAT pin of the device, as under some failure modes of the device, the voltage at the IN pin may appear on the VBAT pin. This voltage can be as high as 30 V, and applying 30 V to the battery in case of the failure of the device and can be hazardous. Connecting the VBAT pin through RBAT prevents a large current from flowing into the battery in case of failure of the device. In the interests of safety, RBAT should have a very high value. The problem with a large RBAT is that the voltage drop across this resistor because of the VBAT bias current IVBAT causes an error in the BVOVP threshold. This error is over and above the tolerance on the nominal 4.35-V BVOVP threshold.

Choosing RBAT in the range from 100 KΩ to 470 kΩ is a good compromise. In the case of a device failure, with RBAT equal to 100 kΩ, the maximum current flowing into the battery would be (30 V – 3 V) ÷ 100 kΩ = 270 μA, which is low enough to be absorbed by the bias currents of the system components. RBAT equal to 100 kΩ would result in a worst-case voltage drop of RBAT × IVBAT = 1 mV. This is negligible compared to the internal tolerance of 50 mV on the BVOVP threshold.

If the Bat-OVP function is not required, the VBAT pin should be connected to VSS.

9.2.2.2 Selection of RCE

The CE pin can be used to enable and disable the device. If host control is not required, the CE pin can be tied to ground or left unconnected, permanently enabling the device.

In applications where external control is required, the CE pin can be controlled by a host processor. As in the case of the VBAT pin (see previous discussion), the CE pin should be connected to the host GPIO pin through as large a resistor as possible. The limitation on the resistor value is that the minimum VOH of the host GPIO pin less the drop across the resistor should be greater than VIH of the bq24308 device's CE pin. The drop across the resistor is given by RCE × IIH.

9.2.2.3 Selection of Input and Output Bypass Capacitors

The input capacitor CIN in Figure 12 and Figure 13 is for decoupling and serves an important purpose. Whenever there is a step change downwards in the system load current, the inductance of the input cable causes the input voltage to spike up. CIN prevents the input voltage from overshooting to dangerous levels. It is strongly recommended that a ceramic capacitor of at least 1 μF be used at the input of the device. It should be located in close proximity to the IN pin.

COUT in Figure 12 and Figure 13 is also important: If a very fast (< 1 µs rise-time) overvoltage transient occurs at the input, the current that charges COUT causes the device’s current-limiting loop to kick in, reducing the gate-drive to FET Q1. This results in improved performance for input overvoltage protection. COUT should also be a ceramic capacitor of at least 1 µF, located close to the OUT pin. COUT also serves as the input decoupling capacitor for the charging circuit downstream of the protection device.

bq24308 typ_app_cir_lus977.gifFigure 12. Overvoltage, Overcurrent, and Battery Overvoltage Protection
bq24308 rev_polarity_lus977.gifFigure 13. OVP, OCP, BATOVP With Input Reverse-Polarity Protection

9.2.2.4 Selection of the PGATE External MOSFET

The PGATE output drives the gate of an external MOSFET to protect the device from reverse polarity input voltages. The MOSFET must be sized to handle the expected current in the application. Additionally, the impedance of the MOSFET is in series with the internal FET of the bq24308, so that the overall acceptable system resistance must be taken into account. Ensure the MOSFET VDS maximum rating exceeds the worst-case expected reverse voltage in the application. The bq24308 withstands up to –30 V, so a 30 V rating on the MOSFET is a good target. The maximum VGS of the MOSFET must be greater than –17 V to ensure operation up to 30 V inputs.

9.2.3 Application Curves

bq24308 npo_ss_lus764.gif
VIN = 0 V to 6 V tR = 20 μs
Figure 14. Normal Power-On Showing Soft-Start
bq24308 ovp_2us_lus977.gif
VIN = 5 V to 8 V tR = 3 μs
Figure 16. OVP Response for Input Step
bq24308 rec_ovp_lus977.gif
VIN = 8 V to 5 V tF = 100 μs
Figure 18. Recovery from Input OVP
bq24308 ocp_blk_lus977.gif
ROUT Switches from 16 Ω to 2.8 Ω
Figure 20. OCP, Showing Current Limiting
bq24308 zoom_lus977.gif
Figure 22. Zoom-in on Turnoff Region of Figure 21, Showing Soft-Stop
bq24308 po_iov_lus764.gif
VIN = 0 V to 12 V tR = 50 μs
Figure 15. Power-On with Input Overvoltage
bq24308 out_lus977.gif
Figure 17. OUT Pin Response to Slow Input Ramp
bq24308 ocp_pu_lus977.gif
Figure 19. OCP, Powering up with OUT Pin Shorted to VSS
bq24308 ocp_ocp_lus977.gif
ROUT Switches from 16 Ω to 2.8 Ω
Figure 21. OCP, Showing Current Limiting and OCP Blanking
bq24308 bat_ovp_lus764.gif
VVBAT Steps from 4.3 V to 4.5 V.
Figure 23. Battery OVP, tDGL(BOVP) and Soft-Stop