处理器

数字信号处理器 - 支持与培训

DSP 按需培训

德州仪器 (TI) 提供各种在线培训和支持,使您可以获得使用 TI DSP 进行成功开发所需的全部信息。

Sitara 处理器按需培训
C66x DSP 架构培训
标题 说明 长度
KeyStone C66x DSP CorePac Overview This module discusses how high performance can be achieved within each C66x DSP core. Topics include C66x DSP CorePac architecture, Single Instruction Multiple Data (SIMD), memory access, and software pipelining. 31 minutes
KeyStone Instruction Set Architecture (ISA) This module describes the differences between the TMS320C674x instruction set architecture and the TMS320C66x instruction set included in the KeyStone CorePac. 31 minutes
Back To Top
C66x DSP 存储器 & 传输培训
标题 说明 长度
KeyStone Multicore Navigator
This module provides an introduction to the architecture and functional components of the Multicore Navigator, which includes the Queue Manager Subsystem (QMSS) and Packet DMA (PKTDMA).
32 minutes
KeyStone Multicore Navigator: Queue Manager Subsystem (QMSS)
This module provides a detailed look at the functional elements of the QMSS and provides information on programming QMSS through the use of registers and low level drivers.
32 minutes
KeyStone Multicore Navigator: Packet DMA This module provides a detailed look at the infrastructure and functional aspects of the PKTDMA and provides information on programming PKTDMA through the use of registers and low level drivers. 24 minutes
KeyStone Inter-Processor Communication (IPC) This module provides an overview of the hardware and software that transports data and/or signals between threads of execution in KeyStone I C66x DSP multicore devices. 40 minutes
Back To Top
C66x DSP 外部接口培训
标题 说明 长度
KeyStone External Interfaces (EMIF-A, UART, I2C, SPI, TSIP)
This module provides an overview of selected external interfaces on KeyStone devices including UART, I2C, SPI, TSIP, and EMIF-A.
22 minutes
KeyStone Serial Rapid IO (SRIO)
This module takes a look at the new features and enhancements of the SRIO on KeyStone devices.
66 minutes
Back To Top
C66x DSP 软件 & 工具培训
标题 说明 长度
Multicore Software Development Kit (MCSDK) for KeyStone Devices
This module provides an overview of the multicore SoC software for KeyStone I C66x DSP devices. This module introduces the optimized software components that enable the rapid development of multicore applications and accelerate time to market using foundational software in the MCSDK. The MCSDK also enables developers to evaluate the hardware and software capabilities using the C66x evaluation module.
17 minutes
KeyStone II Software Overview
Description: This module describes the software development ecosystem for the KeyStone II DSP+ARM multicore devices from both a Linux and SYS/BIOS perspective.
30 minutes
KeyStone Power Management This module provides an overview of the C66x power domain topology, power-saving features, power and clocking domains, power states, and Smart Reflex. 46 minutes
Back to Top

视频

设计网络

德州仪器 (TI) 的开发商网络是由数百家提供支持 TI DSP 的产品和服务的独立公司组成的全球网络。客户可借助以下开发商网络产品简化开发并缩短上市时间:

硬件工具 – 参考设计、开发板/EVM、生产编程工具、设计人员套件和适配器/支持组件

软件工具 – 应用软件、编译器/汇编器/连接器、实时操作系统和开源软件工具

咨询服务 – 全球咨询支持和服务

全球

重要的设计网络合作伙伴

为围绕 TI 平台寻求基于 Windows Embedded、Windows Mobile、Android 和 Linux Embedded 操作系统的解决方案的公司提供世界领先的设计、系统集成、支持和培训专业知识。

率先为 TI 的 DSP 引入 USB JTAG 仿真器,是美国和外国客户的高级仿真产品、专业服务和专门产品提供商。

专门进行电子产品开发的嵌入式系统工程公司,其电子产品可帮助客户将其应用引入科学、工业、通信和运输领域。

D3 Engineering 为数字视频和分析、智能电源管理和精确运动控制的嵌入式产品开发提供领先的快速、低风险路径。

Spectrum Digital, Inc. 设计、开发、制造和销售用于 TI DSP 的工具。产品包括仿真器、评估模块和特定于应用的硬件。

为安全与监控、视频成像、网络与电信、航天与国防、消费类电子产品和医疗保健行业纵向市场提供产品生命周期管理服务。

Enea 拥有范围广泛、内部开发的软件产品系列,包括用于全球半数 3G 手机和基站的操作系统。

一家工程设计服务公司,帮助其他公司设计和开发新的电子设备。擅长从初始概念开始(到原型设计,再到生产)实现产品。

信号处理应用领域的专业公司,专注于媒体处理、无线和通信领域。

Logic PD 由问题解决专家组成的创造性团队以及领先的模块化技术产品可以使客户公司控制成本、降低风险并更快地向市场交付创新型产品。

Mentor Graphics 的一个部门,由优秀的 Linux、Android 和 TI Android Rowboat 开源专家提供有关开发设置的咨询服务,涵盖从产品创建到优化的整个过程。

Mistral 致力于提供产品设计服务、国防解决方案和国家安全解决方案,可以使最终用户和客户加快各种应用的上市步伐,从而从中受益。

Nuvation 的设计和制造团队为高端视频和成像、手持式/便携式消费类和医疗设备以及高性能计算行业提供高级产品解决方案。

提供技术、专业知识和经验以帮助其他公司创建安全可靠的互联系统,通过我们独特的软件平台在消费者和嵌入式世界之间架起一座桥梁。

提供机械、电气和软件工程服务,以解决从概念到制造的及其艰难的挑战。

为数以千计的嵌入式开发人员提供 Linux 产品和服务,是 LinuxLink(一种适用于嵌入式 Linux 应用的高生产力软件开发框架)提供商。

Z3 Technology 提供 OEM 即时可用的硬件模块和特定于应用的软件,包括其嵌入式多媒体播放器、多媒体录制器、流编码器和流接收器应用。

DSP 社区 Wiki & DSP 论坛

Wikis

访问德州仪器 (TI) 嵌入式处理器 Wiki,获取 DSP 技术信息。

 

TI E2E 社区徽标

论坛

与同行工程师交流,咨询问题、共享知识和解决问题。