ZHCU837 December 2021
The magnetic flux density detected at switches U3 and U4 were simulated to determine appropriate placement of the Hall-effect sensors. For simulation, the distance measurements are done with respect to the sensing element to the magnet since the tool does not automatically consider the location of the sensing element within the device.
Figure 2-12 shows the corresponding magnetic flux density graphs for U3 and U4 across the travel distance of the trigger magnet.