TIDUE59A May 2018 – September 2020
To run the demo, the CC3220S LaunchPad kit must be configured with the jumpers highlighted in Figure 3-1 placed. The placement of jumpers on the SOP header depends on whether the software is being debugged or run standalone from the external serial flash.
The CC3220S-LAUNCHXL must be modified when measuring the power consumption of the system. Section 3.2 describes the modification, because the modification is not necessary to run the software application and demonstrate the system.