SWRZ132B September   2022  – December 2023 CC1354P10

PRODUCTION DATA  

  1.   1
  2.   Trademarks
  3. 1Advisories Matrix
  4. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development Support-Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  5. 3Advisories
    1.     Radio_01
    2.     Radio_02
    3. 3.1 Radio_05
    4.     Power_03
    5.     PKA_01
    6.     PKA_02
    7.     I2C_01
    8.     I2S_01
    9.     CPU_Sys_01
    10. 3.2 CPU_04
    11.     Sys_01
    12.     SYSCTRL_01
    13.     IOC_01
    14.     ADC_02
    15.     Flash_02
  6. 4Revision History

Radio_01

Proprietary radio modes: spurious emissions can affect regulatory compliance

Revisions Affected:

Revision C

Details:

When device internal load capacitors are used with the external 48 MHz crystal, energy couples from the crystal oscillator circuit to the RF output. This coupling causes spurious emissions at N × 48 MHz from carrier frequency. This includes, but is not limited to, the frequency bands supported by the device covered by the following regulations:

When using the +14-dBm RF power amplifier

  • ARIB T-108 (Japan)

When using the +20-dBm RF power amplifier

  • 470- to 510-MHz (China) Band
  • FCC CFR47 Part 15 (US)
  • ETSI EN 300 220 (Europe)
  • ETSI EN 300 328 (Europe)
  • ETSI EN 300 440 (Europe)

Workaround:

For compliance with affected standards, external load capacitors might be needed for the 48 MHz crystal to reduce spurious emissions. Internal capacitors (default 7 pF connected capacitance) must then be disconnected internally.

This workaround is implemented by defining the following symbols in the included customer configuration file (ccfg.c) available in the examples:

#define SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA -128 
#define SET_CCFG_MODE_CONF_XOSC_CAP_MOD 0