SWRA603A March   2018  – May 2019 CC1100 , CC1101 , CC110L , CC1120 , CC1121 , CC1125 , CC113L , CC1150 , CC115L , CC1175 , CC1190 , CC1200 , CC1201 , CC1310 , CC1312PSIP , CC1312R , CC1314R10 , CC1350 , CC1352R , CC2530 , CC2531 , CC2538 , CC2540 , CC2541 , CC2590 , CC2591 , CC2592 , CC2640 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP

 

  1.   Debugging Communication Range
  2.   Trademarks
  3. 1Calculate the Theoretical Range
  4. 2Determine Root Cause
  5. 3Measure the Conducted Sensitivity
  6. 4Measure the Conducted Output Power
  7. 5Antenna Measurements
  8. 6Still Issues?
  9. 7References
  10. 8Revision History

Measure the Conducted Sensitivity

  1. Disconnect the antenna and perform conducted measurements at the SMA connector or solder a semi-rigid coax cable at the 50 Ω point.
  2. Preferred: Use a signal generator that is capable of sending data packets. If the signal generator cannot send data packets, just send preamble data.
  3. If a signal generator is not available, use an EM/Launchpad as a transmitter. Use coax cables and attenuation between the EM SMA connector and the 50 Ω point on the custom board.
    Note:

    It is difficult to get an accurate number using this method since the exact values of output power and attenuation are normally not known.

    1. Some energy will also travel over the air from the EM to the DUT. In addition, background noise could impact the results. To get more accurate results, the receiver should be placed in a shielded box.
  4. If the conducted sensitivity is poor:
    1. Are the settings the same as the recommended values from SmartRF™ software? If the sensitivity is good when using SmartRF Studio and not with the settings used for the project the settings has to be evaluated.
    2. What is the frequency difference between the DUT and the signal source? Ensure that the RF frequency of the DUT sending a CW is as expected given the tolerance on the xtal used.
    3. Is the schematic according to the reference design including all component values?
    4. Is the layout according to the reference design?