SSZTCA7 August   2015 LM317A

 

  1.   1
  2.   2
    1.     3
    2. 1. Line Regulation
    3. 2. Load Regulation
    4. 3. Reference Voltage Accuracy
    5.     Additional Resources

Brett Colteaux

GUID-E72B58D1-0DBF-49AA-AFDE-EC5D6150FC10-low.jpg

Would you like your microprocessor to have peak performance all the time? Imagine that the power for your microprocessor consists of a switch mode power supply and a linear regulator, which allows for minimum power consumption. The block diagram for this system can be seen below in Figure 1.

GUID-E4A13094-F7C6-4987-B84E-3581EFB49B78-low.png Figure 1 Microprocessor power supply.

Rapid increases and decreases in current are constantly occurring due to varying processing demands from the microprocessor. In addition, voltage ripple and transient voltages at the output of the switched mode power supply causes varying voltages at the input of the linear regulator. Furthermore, the output voltage can change due to deviations in the internal reference voltage of the regulator.

Now, imagine you are using a linear regulator with maximum specification values of line regulation at 0.07%/V, load regulation at 1.5%, and a reference voltage deviation of 4%. The output voltage of this regulator can deviate by as much as 219 mV while TI’s LM317A for example, has output voltage deviation of just 54.8 mV, as shown in Table 1.

Table 1 TI’s LM317A vs. the typical linear regulator output accuracy.
GUID-15A2B6A1-05F4-4579-A844-537BA7F91C0C-low.png

Note: Conditions used to determine ΔVOUT are 8V ≤ VIN ≤ 24V, 10 mA ≤ IOUT ≤ 1.5A, TJ = 25°C, and VOUT,nominal = 3.3V.

A typical microprocessor desires VCC of 3.3V and maximum VCC of 3.6V. With these specifications taken into consideration, the input voltage of the microprocessor could be up to 3.52V. This leaves only an 80mV margin until the microprocessor stops functioning, which is not enough when considering resistor tolerance values.

The ability to accurately maintain an output voltage is extremely important when it comes to voltage regulators. When choosing a linear voltage regulator for a given application, there are three datasheet specifications that must be scrutinized in order ensure output voltage stability: load regulation, line regulation and reference voltage accuracy.

1. Line Regulation

This specification is used to measure how well a voltage regulator is able to maintain a constant output voltage for input voltage changes. The units of line regulation are expressed in %/V and the value represents the output voltage percent change with respect to input voltage changes. The equation for calculating percent line regulation is as follows:

GUID-266B4B35-4584-484D-A8A0-5B6F70CE8201-low.png

2. Load Regulation

This specification is used to measure how well a voltage regulator is able to maintain a constant output voltage given load changes. Load regulation, which is typically expressed in percent form, is defined by the following equation:

GUID-7F14E137-959A-40BF-8A33-F8D9AD2B8537-low.png

3. Reference Voltage Accuracy

This specification shows the deviation of the internal reference voltage from device to device. It is important that the reference voltage not deviate greatly since its ability to maintain constant depicts how well the regulator can output the desired voltage accurately. The following equation was used to calculate the percent reference voltage accuracy:

GUID-8DBF4811-29AA-4AC5-8321-4219BB2C1CE9-low.png

Additional Resources