SPRACR6 April 2020 TMS320F280023-Q1 , TMS320F280023C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
In this daisy chain network topology as shown in Figure 16 and Figure 17, multiple devices are wired together in a ring topology. Figure 16 shows the connection with 1 data line and Figure 17 shows the same for 2 data lines. Message from master device goes through series of slave devices connected serially. This topology does not pose any limit on the number of devices in the network and amends itself to simple wiring of various nodes. Due to the nature of a daisy-chain connection, data will need to pass through N devices for the transmission before it reaches the last device adding to latency.
In Table 1, it was calculated that a total of seven F28002x MCUs are needed to control 24 MPPT DC/DC boost stages. Therefore, to control 24 MPPT DC/DC boost stages using a daisy chain configuration the transmission delay of all 7 MCUs need to be calculated when the master device (the DC/AC inverter MCU), attempts to communicate with the 7th DC/DC MCU in the chain. This will be the worst case delay in the chain.
For the DPCA inverter system illustrated in Figure 13, the master MCU (F28004x) has only one FSI port. Therefore, in this case, the only way more than one F28002x slave MCUs can be connected in the FSI network is through daisy chain connection.