SPRACM7 December 2020 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
A frequently encountered issue with embedded code development is detecting an overflowing stack. With ERAD, a single enhanced bus-comparator unit can be used., Then, map the stack end address with a small margin to generate an interrupt when there is a write that is attempted. With the example below, just use a comparator with address 0x99FF0 and mask the last 4-bits for comparison. Any write access to 0x99FF0 to 0x99FFF would generate an event/interrupt, which can then be handled appropriately based on kind of the application.
Example: C2000Ware_3_03_00_00\driverlib\<f28004x/f28002x/f2838x>\examples\erad\c28x_hwbp_stack_overflow\erad_ex8_hwbp_stack_threshold_detection.c