SNOSD01D May 2015 – October 2016
PRODUCTION DATA.
For on-line LDC system design tools, see Texas Instruments' Webench® Tool.
The LDC Calculator tools provides a collection of calculation tools which run under MS Excel® useful for LDC system development.
For detailed information on LDC sensor design, refer to the application report LDC Sensor Design.
For detailed information on lateral position sensing with an LDC, in which a target is moved at a constant height from a sensor and the offset is to be measured, refer to LDC1612/LDC1614 Linear Position Sensing. The LDC1101 LHR mode is functionally equivalent to a single channel LDC1612/LDC1614.
For information on temperature compensation, refer to LDC1000 Temperature Compensation.
The following resources contain additional information on LDC1101 operation, configuration, and system design:
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
Webench is a registered trademark of Texas Instruments.
Excel is a registered trademark of Microsoft Corporation.
SPI is a trademark of Motorola.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.