SNAS634B March 2014 – January 2016
PRODUCTION DATA.
Residual Error After One Point Calibration is the error acquired in the Analog Signal Path due to the inaccuracies of the constituent signal processing blocks: DAC, Buffer Amplifier, internal Reference. REAOPC is dominated by the Offset and Gain temperature drifts, since the significant portion of the initial error is eliminated through the One Point Calibration process. The small contribution from the DAC linearity error (INL) is omitted, since it is numerically insignificant. REAOPC can be predicted through the following formulation:
One Point Calibration is the process where the output of the LMP92066 is adjusted in the target system to achieve the desired response, at temperature T0. Typically this involves measurement of the overall system output variable; for example, ID of the PA, and modification of the BASE value in the LUT to achieve the desired PA bias current.
PowerPAD is a trademark of Texas Instruments Incorporated.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.