SLVSDU6D July 2017 – November 2019
PRODUCTION DATA.
Though ATL431LI is stable with no capacitive load, the device that receives the shunt regulator's output voltage could present a capacitive load that is within the ATL431LI region of stability, shown in Figure 13. Also, designers may use capacitive loads to improve the transient response or for power supply decoupling. When using additional capacitance between Cathode and Anode, see Figure 13. Also, application note Understanding Stability Boundary Conditions Charts in TL431, TL432 Data Sheet, SLVA482 will provide a deeper understanding of this devices stability characteristics and aid the user in making the right choices when choosing a load capacitor.