SLVAEV6 December   2020 DRV8702-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the DRV8702-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

These PIN FMA tables also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the DRV8702-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the DRV8702-Q1 data sheet.

GUID-D3EF2492-9B94-46E3-966E-C21A6608AE71-low.svg Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device is used with external components consistent with the values described in the external component table of the datasheet.

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
GND 1 Intended operation D
IN1/PH 2 Gate driver input control stuck low. Driver output may not match input. B
IN2/EN 3 Gate driver input control stuck low. Driver output may not match input. B
GND 4 Intended operation D
IDRIVE 5 Device IDRIVE setting potentially incorrect B
VDS 6 Device VDS setting potentially incorrect B
GND 7 Intended operation D
nSLEEP 8 Device stuck in sleep state. Outputs non-operational. B
GND 9 Intended operation D
nFAULT 10 Device fault output indicator always active. B
MODE 11 Device MODE setting potentially incorrect. B
DVDD 12 Device external digital power supply stuck low. Device non-operational. B
GND 13 Intended operation D
AVDD 14 Device non-operational. Power dissipation through AVDD B
VREF 15 Current limit will trip every cycle B
SO 16 Device current sense feedback invalid. B
GND 17 Intended operation D
GH1 18 HS1 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
SH1 19 HS1 MOSFET non-functional. Device will report VDS fault B
GL1 20 LS1 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
SP 21 Device current sense feedback invalid. B
SN 22 Device current sense feedback invalid. B
SL2 23 Sense amplifier output is always low, no current regulation B
GL2 24 LS2 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
SH2 25 HS2 MOSFET non-functional. Device will report VDS fault B
GH2 26 HS2 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
VDRAIN 27 Device overcurrent monitors and open load diagnostic non-operational. B
PVDD 28 Device external power supply stuck low. Device gate drivers and shunt amplifier non-operational. B
VCP 29 Device will be damaged A
CPH 30 Device will be damaged A
CPL 31 Device will report a charge pump fault A
NC 32 No effect B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
GND1Device behavior undefined, may retain operation due to alternative GND pin.C
IN1/PH2Gate driver input control missing. Driver output may not match input.B
IN2/EN3 Gate driver input control missing. Driver output may not match input.B
GND 4 Device behavior undefined, may retain operation due to alternative GND pin. C
IDRIVE 5 Device IDRIVE setting potentially incorrect B
VDS 6 Device VDS setting potentially incorrect B
GND 7 Device behavior undefined, may retain operation due to alternative GND pin. C
nSLEEP 8 Device stuck in sleep state. Outputs non-operational. B
GND 9 Device behavior undefined, may retain operation due to alternative GND pin. C
nFAULT 10 Device fault output indicator invalid. B
MODE 11 Device MODE setting potentially incorrect. B
DVDD 12 Device external digital power supply missing. Device non-operational. B
GND 13 Device behavior undefined, may retain operation due to alternative GND pin. C
AVDD 14 Device behavior undefined, regulator may not be stable. B
VREF 15 Current limit will be unstable B
SO 16 Device current sense feedback invalid. B
GND 17 Device behavior undefined, may retain operation due to alternative GND pin. C
GH1 18 HS1 MOSFET off B
SH1 19 HS1 MOSFET non-functional, Device will report VDS fault B
GL1 20 LS1 MOSFET off B
SP 21 Device current sense feedback invalid. B
SN 22 Device current sense feedback invalid. B
SL2 23 Device will report a VDS fault B
GL2 24 LS2 MOSFET off B
SH2 25 HS2 MOSFET non-functional, Device will report VDS fault B
GH2 26 HS2 MOSFET off B
VDRAIN 27 Device overcurrent monitors and open load diagnostic non-operational. B
PVDD 28 Device external power supply missing. Device gate drivers and shunt amplifier non-operational. B
VCP 29 Charge pump undervoltage and gate drivers disabled. B
CPH 30 Charge pump undervoltage and gate drivers disabled. B
CPL 31 Charge pump undervoltage and gate drivers disabled. B
NC 32 Intended operation B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
GND12Logic operation is changed. Driver output may not match input.B
IN1/PH23Logic operation is changed. Driver output may not match input.B
IN2/EN34Logic operation is changed. Driver output may not match input.B
GND 4 5 Increased switching losses in FETs or gate drive fault B
IDRIVE 5 6 Device IDRIVE and VDS setting potentially incorrect B
VDS 6 7 Device VDS setting potentially incorrect B
GND 7 8 Device stuck in sleep state. Outputs non-operational. B
nSLEEP 8 9 Device stuck in sleep state. Outputs non-operational. B
GND 9 10 Device fault output indicator always active. B
nFAULT 10 11 MODE will change to PH/EN whenever a FAULT occurs and nSLEEP toggled B
MODE 11 12 Device MODE setting potentially incorrect. B
DVDD 12 13 Device external digital power supply missing. Device non-operational. B
GND 13 14 Device non-operational. Power dissipation through AVDD B
AVDD 14 15 Current regulation disabled B
VREF 15 16 Device current sense feedback invalid. B
SO 16 17 Device current sense feedback invalid. B
GND 17 18 HS1 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
GH1 18 19 HS1 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
SH1 19 20 GL1 output invalid, may violate GL1 abs max. A
GL1 20 21 LS1 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
SP 21 22 Device current sense feedback invalid. B
SN 22 23 Device current sense feedback invalid. B
SL2 23 24 LS2 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
GL2 24 25 GL2 output invalid, may violate GL2 abs max. A
SH2 25 26 HS2 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
GH2 26 27 HS2 MOSFET off, energy limited by TDRIVE. Device will report VGS fault B
VDRAIN 27 28 Hard short instead of a kelvin connection may degrate VDS accuracy B
PVDD 28 29 Device will report a charge pump fault A
VCP 29 30 Device will not power up A
CPH 30 31 Device will report a charge pump fault A
CPL 31 32 No effect B
NC 32 1 No effect B