SLVAEK4B January   2020  – June 2021 TPS4H160-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)
  6. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TPS4H160-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the TPS4H160-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS4H160-Q1 data sheet.

Figure 4-1 Pin Diagram (Version A)
Figure 4-2 Pin Diagram (Version B)

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Follows data sheet recommendation for operating conditions, external components selection and PCB layout.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
GND1, 12Resistor/diode network will be bypassed if present.B
NC2, 19, 24No effect.D
INx3, 4, 5, 6Shutdown of corresponding channel.B
STx7, 8, 9, 10Version A only. Status being reported may be erroneous.B
SEH7Version B only. If DIAG_EN is high then only channel 3 or 4's (depending on SEL) sense current output will be on SNS pin.B
SEL8Version B only. If DIAG_EN is high then only channel 1 or 2's (depending on SEH) sense current output will be on SNS pin.B
FAULT9Version B only. Status being reported may be erroneous.
CS10Version B only. Sense current not valid from CS pin.B
CL11Device will default to internal current limit.C
THER13Device will default to "auto-retry" mode when encountering thermal fault.B
DIAG_EN14Diagnostics will be disabled.B
OUTx15,16,17, 18, 25, 26, 27, 28Current limit of device will engage.B
VS20, 21, 22, 23Device will have no input supply and therefore not function.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
GND1, 12Loss of ground detection engages and device shuts off.B
NC2, 19, 24No effect.D
INx3, 4, 5, 6Corresponding channel will be shutdown and INx will be pulled down internally.B
STx7, 8, 9, 10Version A only. STx pin cannot pull high and diagnostics cannot be reported.B
SEH7Version B only. Pulled low internally, however wrong SNS current potentially reported on CS if DIAG_EN is high.B
SEL8Version B only. If DIAG_EN is high then only channel 1 or 2's (depending on SEH) sense current output will be on SNS pin.B
FAULT9Version B only. Fault signal not reported.B
CS10Version B only. Correct sense current cannot be read.B
CL11Device will default to internal current limit.C
THER13Internally pulled down. Device will default to "auto-retry" mode when encountering thermal fault.B
DIAG_EN14Internally pulled down. Diagnostics will be disabled.B
OUTx15, 16, 17, 18, 25, 26, 27, 28No effect. If configured, open load detection will trigger.B
VS20, 21, 22, 23Device will have no input supply and therefore not function.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
GND1NCNo effect.D
NC2IN1No effect.D
IN13IN2IN1 signal will affect IN2 signal and vice versa.B
IN24IN3IN2 signal will affect IN3 signal and vice versa.B
IN35IN4IN3 signal will affect IN4 signal and vice versa.B
IN46ST1Version A only. If ST1 is high then channel 4 will be on.B
IN46SEHVersion B only. IN4 signal will affect SEH and vice versa.B
ST17ST2Version A only. Fault reporting of channel 1 and channel 2 may be erroneous. B
SEH7SELVersion B only. SEH signal will affect SEL and vice versa. If DIAG_EN is high only channel 1 or 4 can be read at SNS.B
ST28ST3Version A only. Fault reporting of channel 2 and channel 3 may be erroneous.B
SEL8FAULTVersion B only. If FAULT high and DIAG_EN high, only channel 2 or channel 4 can be read at SNS.B
ST39ST4Version A only. Fault reporting of channel 3 and channel 4 may be erroneous. B
FAULT9CSVersion B only. Fault reporting and current sense reporting will be erroneous.B
ST410CLVersion A only. ST4 voltage could cause erroneous current limit to be set on device.B
CS10CLVersion B only. Voltage level on CS could cause erroneous current limit to be set on device.B
CL11GNDDevice will default to internal current limit.C
GND12THERDevice will be in "auto-retry" mode when encountering a thermal fault.B
THER13DIAG_ENTHER signal will affect DIAG_EN signal and vice versa.B
OUT415OUT4No effectD
OUT416OUT3Output of channel 4 will be tied to output of channel 3.B
OUT317OUT3No effect.D
OUT318NCNo effect.D
NC19VSNo effect.D
VS20VSNo effect.D
VS23NCNo effect.D
NC24OUT2No effect.D
OUT225OUT2No effect.D
OUT226OUT1Output of channel 2 will be tied to output of channel 1.B
OUT127OUT1No effect.D
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply (VS)
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
GND1, 12Supply power will be bypassed and device will not turn on.B
NC2, 19, 24No effect. D
INx3, 4, 5, 6Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
STx7, 8, 9, 10Version A only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
SEH7Version B only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cellA
SEL8Version B only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
FAULT9Version B only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
CS10Version B only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
CL11Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
THER13Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
DIAG_EN14Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell.A
OUTx15, 16, 17, 18, 25, 26, 27, 28Output will be pulled to supply voltage. Short-to-battery detection will be triggered if configured.B