SLUAAG8 October 2022 TPS56C231
In Cadence simulator, Virtuoso ADE Product Suite or Spectre X Simulator, using same parameters as Table 2-3, the load transient simulation waveform is shown in Figure 2-9.
Next step is saving Cadence simulation waveform to CSV file. On the top menu, click Trace, then choose Export, and in the pop up window, select the files of type to CSV, change other setup parameters as needed, click Save, as shown in Figure 2-10.