SLOA212A December   2014  – February 2016 RF430FRL152H

 

  1.   Battery-Less NFC/RFID Temperature Sensing Patch
    1.     Trademarks
    2. 1 Reference Design Hardware
    3. 2 Firmware Implementation
    4. 3 Demonstration With TRF7970AEVM
    5. 4 Antenna Design
    6. 5 References
  2.   Revision History

Antenna Design

The antenna coil inductance is measured at 1.84 µH as shown in Figure 7. To calculate the parallel tuning capacitors required, the resonant frequency formula in Equation 1 should be used. For further details on antenna tuning, see the RF430CL330H Practical Antenna Design Guide (SLOA197).

Equation 1. eq1_sloa212.gif
Figure08_SLOA212.gifFigure 7. Coil Inductance

Figure 8 shows the measured resonant frequency at 13.66 MHz with 274.3 kHz. This results in a Q factor of less than 50 using the calculation shown in Equation 2. The read range of this reference board is 8cm using the TRF7970AEVM reader.

Equation 2. eq2_sloa212.gif
Figure10_SLOA212.gifFigure 8. Resonant Frequency