SFFS822 March   2024 SN74AXC8T245-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 TSSOP Package
    2. 2.2 VQFN Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the SN74AXC8T245-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the SN74AXC8T245-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the SN74AXC8T245-Q1 data sheet.

GUID-A788876D-937B-4607-B16F-C99560DABC41-low.gifFigure 4-1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1GND short to VCC, device will be bypassed - may cause system damage, but not device damageB
DIR2Direction control will fix B --> A directionB
A1 - A83 - 10If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
GND11 - 13Normal OperationD
B8 - B114 - 21If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
OE (active low)22Outputs will remain enabledB
VCCB23-24GND short to VCC, device will be bypassed - may cause system damage, but not device damageB
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Device will not be poweredB
DIR2Direction control will fix B --> A directionB
A1 - A83 - 10If configured as output, normal operation. If configured as input, no damage, but output will not switchB
GND11 - 13Device will not be poweredB
B8 - B114 - 21If configured as output, normal operation. If configured as input, no damage, but output will not switchB
OE (active low)22Outputs will remain enabledB
VCCB23-24Device will not be poweredB
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VCCA1DIRDirection control will fix A --> B directionB
DIR2A1If DIR is LOW, A1 will be an output and damage is possible. If DIR is HIGH, A1 will be an input and drive the output B1 low.A
A(n)3 - 9A(n+1)If A(n) and A(n+1) are configured as outputs then damage is possible. If configured as inputs, both bits will have the same value alwaysA
A810GNDIf A8 is configured as an output then damage is possible. If configured as input, output B8 will be fixed lowA
GND11 - 12GNDNormal OperationD
GND13B8If B8 is configured as an output then damage is possible. If configured as input, output A8 will be fixed lowA
B(n)14 - 20B(n-1)If B(n) and B(n+1) are configured as outputs then damage is possible. If configured as inputs, both bits will have the same value alwaysA
B121VCCBIf B1 is configured as an output then damage is possible. If configured as input, no damage, but output A1 will remain high.A
VCCB22-23VCCBNormal OperationD
VCCB24VCCAVCCB short to VCCA, device will be bypassed - may cause system damage, but not device damageB
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCCA
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Normal OperationD
DIR2Direction control will fix A --> B directionB
A1 - A83 - 10If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
GND11 - 13GND short to VCC, device will be bypassed - may cause system damage, but not device damageB
B8 - B114 - 21If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL not metA
OE (active low)22Outputs will remain disabledB
VCCB23-24VCCA short to VCCB, device will be bypassed - may cause system damage, but not device damageB
Table 4-6 Pin FMA for Device Pins Short-Circuited to VCCB
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1VCCB short to VCCA, device will be bypassed - may cause system damage, but not device damageB
DIR2If VCCA > VCCB, then the direction control will fix B-->A, If VCCA < VCCB, damage is possible if VIH/VIL not metA
A1 - A83 - 10If A1 is configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL not metA
GND11 - 13GND short to VCC, device will be bypassed - may cause system damage, but not device damageB
B8 - B114 - 21If B2 is configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
OE (active low)22If VCCA > VCCB, then the outputs will remain disabled, If VCCA < VCCB, damage is possible if VIH/VIL not metA
VCCB23-24Normal OperationD