SFFS624 March 2024 MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0G3507-Q1
The SoC has a couple of registers (SHUTDNSTOREx) which retain their content during SHUTDOWN mode. Since there is no active state monitoring by the CPU possible in SHUTDOWN mode, a parity protection has been added to these registers. On the detection of a parity error, the PMU will issue a POR reset request. If the device was in SHUTDOWN mode, the device will not reset right away. The device will wakeup with a next wakeup event and the PMU will issue the POR request and clear the SHUTDNSTOREx registers. The SW will see this wakeup as POR reset, rather then a wakeup from SHUTDOWN mode, which indicates the content in the SHUTDNSTOREx registers has been reset.