All trademarks are the property of their respective owners.
Guarding is a PCB layout technique that helps shield sensitive nets from parasitic circuit elements or external influences that can cause noise or leakages which can impact the performance of an application. These leakages can be from a multitude of sources, however, applications requiring the most accurate solutions need to consider all potential leakage sources. A model of adjacent trace parasitics and possible environment influences can be seen in Figure 1-1 (top view).
As seen above, leakage paths can be formed from several sources including flux on the board, debris (surface leakages), electrical interferences, and of course the inherent board resistance and dielectrics between conductors (traces in this case). Now, while the first two can be removed by having clean manufacturing processes and operational areas or burying the sensitive traces within the PBC, the third and fourth instances can affect any PCB and can cause significant leakages to form if proper guarding is not implemented into the design.
Take the trace to trace resistance as an example. At just a 5 V potential difference between two traces on a PCB and using an estimated trace to trace resistance in the Gigaohm range, this would amount to nA's worth of leakage just from this relatively small delta alone. So one can imagine the increased leakage the net would see from any substantial increase in voltage present on the board. Hence why incorporating a guarding scheme can be so important to keep leakage currents at bay.
Guarding techniques implement active conductors that are at the same potential as the sensitive net and surround said net to create an extremely low leakage environment. With the guard ring and the net at the same potential, this effectively creates an incredibly small voltage delta between the trace and immediate surrounding area which drastically reduces the possibility of stray leakage currents leaking into this area of the PCB. Figure 1-2 outlines a typical guarding scheme.
To ensure the highest level of leakage performance, there are some best practices for guarding that should be adhered to. As mentioned earlier, the first barrier that needs to be protected again is surface contamination that can often lead to stray leakage currents. In order to counteract this, it is best to bury sensitive nets within the PCB itself to reduce the possibility of any type of debris or contamination from providing leakage paths to the sensitive nets. To go even further, the next recommendation would be to implement a “boxing” ring around the entire net. What this means is that in addition to the traditional guarding which is just on the same layer as the net, the layers above and below also provide shielding by being at the same potential as the guard traces. This type of configuration will mimic the effects of a shielding cable in which it shields the net 360°. Figure 2-1 provides a visual representation.
With package sizes becoming smaller and smaller, this can introduce challenges in incorporating a full guard ring on the trace due to the pitch of some packages. To address this, the designer will need to run the guard ring and traces as close to the pin as possible while still leaving some space between the adjacent guard traces (see Figure 2-2).
However, if a full guard is required, TI does offer devices that are more guarding friendly in SOIC packages. These are wider pitch devices which will allow for a full guard to be implemented around each pin of the device. One such example can be seen using the MUX36S16DWR, as shown in Figure 2-3.
Lastly, the design must ensure that the guard is well generated. What this means is that the guard voltage mimics the net voltage as closely as possible to provide the optimal guarding results. To do this, one must just simply incorporate a precision buffer to be able to drive the guard appropriately. Figure 2-4 illustrates a sample topology.
This topology is recommended to be designed with a precision buffer to reduce any extra leakage currents emanating from the op-amp itself and to ensure the closest guard possible. Table 2-1 shows some recommended op-amps to use for this application.
Device | Voltage Range |
Offset Voltage |
---|---|---|
OPA397 | 5.5 V | 60 uV |
OPAx197 | 36 V | 25 µV |
OPA593 | 85 V | 10 µV |
OPA455 | 150 V | 3.4 mV |
Leakage currents introduced from multiplexers can contribute to undesirable results when implemented into a high precision application. Table 3-1 shows that there are two different multiplexers to choose from.
Multiplexer | Leakage Performance (25C/125C) | On-Resistance (25C/125C) |
---|---|---|
TMUX1108 | 3pA/950pA | 2.5 Ω/4.9 Ω |
TMUX1308 | 1nA/800nA | 75 Ω/270 Ω |
These devices will have leakage and resistance components to them that can have an influence on the application and contribute error if proper guarding precautions are not put into place. The error that is introduced from these leakage currents is equivalent to the approximate amount shown in Equation 1.
To further clarify, the model of a multiplexer’s ON leakage current is shown in Figure 3-1.
When feeding into a high impedance node, the leakage current takes the path of least resistance, which is through the on-resistance and source-resistance path and induce an offset error that affects the measurement at the output. Continuing using the chosen multiplexers above, it is evident that leakage can indeed be significant if proper guarding and device selection is not taken into serious consideration (below is assuming Rsource is negligible).
Multiplexer | Leakage Performance (25°C/125°C) | On-Resistance (25°C/125°C) | Offset Error (25°C/125°C) |
---|---|---|---|
TMUX1108 | 3 pA/950 pA | 2.5 Ω/4.9 Ω | 7.5 pV/4.6 nV |
TMUX1308 | 1nA/800 nA | 75 Ω/270 Ω | 75 nV/216 µV |
While this example above showcases how leakage currents can contribute heavily to offset error just based on multiplexer selection, it is important to note that the low leakage performance can only be achieved with a proper layout and guarding implemented.
While guarding plays a critical role in determining the leakage performance of certain applications, the application needs to start with a very high precision capable device in order to achieve such low levels of leakage. TI offers several different multiplexer families that would be recommended in such applications as shown in Table 4-1.
Device | Configuration | Voltage Range | On-Leakage (25°C) | On-Resistance (25°C) |
---|---|---|---|---|
TMUX1108/09 | 8:1x1/4:1x2 | 5 V, ±2.5 V | 3pA | 2.5 Ω |
TMUX1111/2/3 | 1:1x4 | 5 V | 3 pA | 2.5 Ω |
TMUX1121/2/3 | 1:1x2 | 5 V | 3 pA | 1.9 Ω |
TMUX6111/2/3 | 1:1x4 | 17 V, ±17 V | 10 pA | 125 Ω |
TMUX6121/2/3 | 1:1x2 | 17 V, ±17 V | 10 pA | 120 Ω |
MUX36D08 | 8:1x2 | 36 V, ±18 V | 10 pA | 125 Ω |
MUX36S16 | 16:1x1 | 36V, ±18 V | 10 pA | 125 Ω |
TMUX7219 | 2:1x1 | 44 V, ±22 V | 40 pA | 2.1 Ω |
TMUX7208/09 | 8:1x1/4:1x2 | 44 V, ±22 V | 40 pA | 4 Ω |
TMUX7211/2/3 | 1:1x4 | 44 V, ±22 V | 100 pA | 1.7 Ω |
TMUX8108/09 | 8:1x1/4:1x2 | 100 V, ±50 V | 40 pA | 38 Ω |
TMUX8211/2/3 | 1:1x4 | 100 V, ±50 V | 10 pA | 5 Ω |
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 Copyright © 2022, Texas Instruments Incorporated |