SBAA541 December 2022 AMC1202 , AMC1302 , AMC1306M05 , AMC22C11 , AMC22C12 , AMC23C10 , AMC23C11 , AMC23C12 , AMC23C14 , AMC23C15 , AMC3302 , AMC3306M05
In this application note, only shunt-based current sensing with isolated amplifiers or isolated delta-sigma modulators are considered. All products discussed have a linear input voltage range of ±50 mV which allows use of very small shunt-resistor values to keep power a low energy dissipation compared to the overall power of the system.
In the reference application, for an 11-kW AC/DC, the input currents have a maximum value or 16 ARMS for 400 VAC three-phase system. This results in ±22.5 Apeak. With a 2-mΩ shunt resistor, the maximum voltage across the shunt can be kept well below 50 mV (peak is 45 mV), meaning that at maximum power operation of 11 kW the power dissipation within the shunt is only 0.5 W per shunt. Assuming three shunts in a 3-phase system this is still negligible loss and does not add any important hot spot on the PCB. Conversely, the currents in the DC/DC converter can be as high as 44 A as indicated in Table 1-1. This result drives the requirements to select a 1-mΩ shunt resistor for the 50-mV input voltage range of the isolated amplifier which results in a power dissipation lower than 2 W for each measurement point (negligible with respect to 11-kW total power).