DLPU115 January   2022 DLPC3421

 

  1.   1
  2.   2
    1.     3
    2.     4
      1.      5
      2.      6
      3.      7
  3.   8
    1.     9
    2.     10
  4.   11
    1.     12
      1.      13
        1.       14
        2.       15
      2.      16
        1.       17
        2.       18
        3.       19
      3.      20
        1.       21
        2.       22
      4.      23
        1.       24
        2.       25
        3.       26
      5.      27
        1.       28
        2.       29
      6.      30
        1.       31
        2.       32
        3.       33
      7.      34
        1.       35
        2.       36
      8.      37
        1.       38
        2.       39
        3.       40
      9.      41
        1.       42
        2.       43
      10.      44
        1.       45
        2.       46
        3.       47
      11.      48
        1.       49
        2.       50
      12.      51
        1.       52
        2.       53
        3.       54
      13.      55
        1.       56
        2.       57
        3.       58
      14.      59
        1.       60
        2.       61
      15.      62
        1.       63
        2.       64
        3.       65
      16.      66
        1.       67
        2.       68
      17.      69
        1.       70
        2.       71
        3.       72
      18.      73
        1.       74
        2.       75
      19.      76
        1.       77
        2.       78
        3.       79
      20.      80
        1.       81
        2.       82
        3.       83
      21.      84
        1.       85
        2.       86
        3.       87
      22.      88
        1.       89
        2.       90
      23.      91
        1.       92
        2.       93
        3.       94
      24.      95
        1.       96
        2.       97
        3.       98
      25.      99
        1.       100
        2.       101
      26.      102
        1.       103
        2.       104
        3.       105
      27.      106
        1.       107
        2.       108
      28.      109
        1.       110
        2.       111
        3.       112
      29.      113
        1.       114
        2.       115
      30.      116
        1.       117
        2.       118
      31.      119
        1.       120
        2.       121
        3.       122
      32.      123
        1.       124
        2.       125
    2.     126
      1.      127
        1.       128
        2.       129
      2.      130
        1.       131
        2.       132
        3.       133
      3.      134
        1.       135
        2.       136
      4.      137
        1.       138
        2.       139
        3.       140
      5.      141
        1.       142
        2.       143
      6.      144
        1.       145
        2.       146
        3.       147
      7.      148
        1.       149
        2.       150
        3.       151
      8.      152
        1.       153
        2.       154
      9.      155
        1.       156
        2.       157
        3.       158
      10.      159
        1.       160
        2.       161
        3.       162
    3.     163
      1.      164
        1.       165
        2.       166
      2.      167
        1.       168
        2.       169
        3.       170
      3.      171
        1.       172
        2.       173
      4.      174
        1.       175
        2.       176
        3.       177
      5.      178
        1.       179
        2.       180
      6.      181
        1.       182
        2.       183
        3.       184
      7.      185
        1.       186
        2.       187
      8.      188
        1.       189
        2.       190
        3.       191
    4.     192
      1.      193
        1.       194
        2.       195
      2.      196
        1.       197
        2.       198
        3.       199
      3.      200
        1.       201
        2.       202
      4.      203
        1.       204
        2.       205
        3.       206
      5.      207
        1.       208
        2.       209
      6.      210
        1.       211
        2.       212
        3.       213
      7.      214
        1.       215
        2.       216
      8.      217
        1.       218
        2.       219
        3.       220
    5.     221
      1.      222
        1.       223
        2.       224
        3.       225
      2.      226
        1.       227
        2.       228
        3.       229
      3.      230
        1.       231
        2.       232
        3.       233
      4.      234
        1.       235
        2.       236
        3.       237
      5.      238
        1.       239
        2.       240
        3.       241
      6.      242
        1.       243
        2.       244
        3.       245
      7.      246
        1.       247
        2.       248
        3.       249

Write Parameters

Table 3-37 describes the command parameters.

Table 3-37 Write Parameters
Parameter BytesDescription
Byte 1See Figure 3-53
Byte 2Optical throw ratio (LSByte)
Byte 3Optical throw ratio (MSByte)
Byte 4Optical DMD offset (LSByte)
Byte 5Optical DMD offset (MSByte)
Figure 3-53 Byte 1 Write Parameters
MSBByte 1LSB
b7b6b5b4b3b2b1b0
b(7:1)

Reserved

b(0)Keystone correction enable:
  • 0: Disabled
  • 1: Enabled

Keystone correction digitally compensates for distorted images when the projector is tilted up or down. Keystone correction is specified by the pitch angle (described in the Write Keystone Projection Pitch Angle command) and based on the throw ratio, vertical offset, and projector orientation. Each parameter is provided by this command. With this information, keystone correction corrects for both overall and local area aspect ratio distortion. For both full screen images and sub-images, the full active area of the DMD is keystone-corrected.

When keystone correction is enabled, the Write Border Color command sets the border color to black. Setting this parameter to any other color produces undesirable results.

Image rotation is allowed while keystone correction is enabled, but it may not be appropriate for all situations or configurations. The user is responsible for determining if the result is acceptable.

Figure 3-54 shows the bit order and weighting for the optical throw ratio data. Figure 3-55 defines how this data is determined.

Figure 3-54 Bit Weight Definition for the Optical Throw Ratio Data
b15b14b13b12b11b10b9b8b7b6b5b4b3b2b1b0
27262524232221202–12–22–32–42–52–62–72–8
GUID-C53DEB53-4ED1-4FC5-A8AC-977E78F7023B-low.gifFigure 3-55 Visual Definition and Calculation for Optical Throw Ratio Data

Figure 3-56 shows the bit order and weighting for the two’s complement optical DMD offset data. Figure 3-57 shows how this data is calculated, while Figure 3-58 shows how the sign of the offset data is determined. The user must insure that both the value and the sign of the offset data are correctly determined.

Figure 3-56 Bit Weight Definition for the Optical DMD Offset Data
b15b14b13b12b11b10b9b8b7b6b5b4b3b2b1b0
27262524232221202–12–22–32–42–52–62–72–8
GUID-993A92AE-107F-41FE-A5A8-C0E52E885EB4-low.gifFigure 3-57 Method for Calculation for Optical DMD Offset Data
GUID-4894D075-115B-44A7-A489-0D34D5C193F3-low.gifFigure 3-58 Sign Determination for Optical DMD Offset Data

Figure 3-59 shows examples of non-inverted and inverted projector orientation. This information is required for byte 1 of this command.

GUID-4BB6430D-64C5-45C5-B1BA-82AFA30371E1-low.gifFigure 3-59 Examples of Non-Inverted and Inverted Projector Orientations