ZHCSJ23C November 2018 – September 2019 UCC20225-Q1 , UCC20225A-Q1
PRODUCTION DATA.
It is recommended that users avoid shaping the signals to the gate driver in an attempt to slow down (or delay) the signal at the output. However, a small input RIN-CIN filter can be used to filter out the ringing introduced by non-ideal layout or long PCB traces.
Such a filter should use an RIN in the range of 0-Ω to 100-Ω and a CIN between 10-pF and 100-pF. In the example, an RIN = 51-Ω and a CIN = 33-pF are selected, with a corner frequency of approximately 100-MHz.
When selecting these components, it is important to pay attention to the trade-off between good noise immunity and propagation delay.