ZHCSH55B December 2017 – September 2018 TPS65218D0
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
Depending on the slew rate of the input voltage into the IN_BIAS pin, the power rails of TPS65218D0 will be enabled at either VULVO or VULVO + VHYS.
If the slew rate of the IN_BIAS voltage is greater than 30 V/s, then TPS65218D0 will power up at VULVO. Once the input voltage rises above this level, the input voltage may drop to the VUVLO level before the PMIC shuts down. In this scenario, if the input voltage were to fall below VUVLO but above 2.55 V, the input voltage would have to recover above VUVLO in less than 5 ms for the device to remain active.
If the slew rate of the IN_BIAS voltage is less than 30 V/s, then TPS65218D0 will power up at VULVO + VHYS. Once the input voltage rises above this level, the input voltage may drop to the VUVLO level before the PMIC shuts down. In this scenario, if the input voltage were to fall below VUVLO but above 2.5 V, the input voltage would have to recover above VUVLO + VHYS in less than 5 ms for the device to remain active.
In either slew rate scenario, if the input voltage were to fall below 2.5 V, the digital core is reset and all remaining power rails are shut down instantaneously and are pulled low to ground by their internal discharge circuitry (DCDC1-4, and LDO1).
After the UVLO triggers, the internal LDO blocks current flow from its output capacitor back to the IN_BIAS pin, allowing the digital core and the discharge circuits to remain powered for a limited amount of time to properly shut-down and discharge the output rails. The hold-up time is determined by the value of the capacitor connected to INT_LDO. See Section 5.3.1.6 for more details.