Power-good (PGOOD) is an open-drain
output of the built-in voltage supervisor that monitors DCDC1, DCDC2, DCDC3, DCDC4,
and LDO1. The output is Hi-Z when all enabled rails are in regulation and driven low
when one or more rails encounter a fault which brings the output voltage outside the
specified tolerance range. In a typical application PGOOD drives the reset signal of
the SOC.
The following rules apply to the PGOOD
output:
- The power-up default state
for THE PGOOD is low. When all rails are disabled, the PGOOD output is
driven low.
- Only enabled rails are
monitored. Disabled rails are ignored.
- Power-good monitoring of a
particular rail starts 5 ms after the rail is enabled and is continuously
monitored thereafter. This allows the rail to power-up.
- The PGOOD is delayed by PGDLY
time after the sequencer is finished and the last rail is enabled.
- If an enabled rail is
continuously outside the monitoring threshold for longer than the deglitch
time, then the PGOOD is pulled low, and all rails are shut-down following
the power-down sequence. PGDLY does not apply.
- Disabling a rail manually by
resetting the DCx_EN or LDO1_EN bit has no effect on the PGOOD pin. If all
rails are disabled, the PGOOD is driven low as the last rail is
disabled.
- If the power-down sequencer
is triggered, PGOOD is driven low.
- The PGOOD is driven low in
the SUSPEND state, regardless of the number of rails that are enabled.
#SLDS2067476 shows a typical power-up sequence and PGOOD timing.