ZHCSNV8A December 2021 – June 2022 TPS63901
PRODUCTION DATA
The device turns on when all of the following conditions are true:
The device turns off when at least one of the following conditions is true:
Figure 7-13 shows a complete state diagram.
After the device turns on, the internal reference system starts, then the trimming information and the CFG pins are read out. The device ignores any further changes to the CFG pins during device operation.
Figure 7-5 shows the internal start-up sequence.