ZHCSGE4B December   2010  – March 2017 TPS61240-Q1
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
    6. 6.6 Typical Characteristics
  7. Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Current Limit Operation
      2. 7.3.2 Undervoltage Lockout
      3. 7.3.3 Input Overvoltage Protection
      4. 7.3.4 Enable
      5. 7.3.5 Soft Start
      6. 7.3.6 Load Disconnect
      7. 7.3.7 Thermal Shutdown
    4. 7.4 Device Functional Modes
      1. 7.4.1 Power-Save Mode
  8. Application and Implementation
    1. 8.1 Application Information
    2. 8.2 Typical Applications
      1. 8.2.1 Design Requirements
      2. 8.2.2 Detailed Design Procedure
        1. 8.2.2.1 Programming the Output Voltage
        2. 8.2.2.2 Inductor Selection
        3. 8.2.2.3 Input Capacitor
        4. 8.2.2.4 Output Capacitor
        5. 8.2.2.5 Checking Loop Stability
      3. 8.2.3 Application Curves
    3. 8.3 System Example
  9. Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11器件和文档支持
    1. 11.1 文档支持
      1. 11.1.1 相关文档
    2. 11.2 接收文档更新通知
    3. 11.3 社区资源
    4. 11.4 商标
    5. 11.5 静电放电警告
    6. 11.6 Glossary
  12. 12机械、封装和可订购信息

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

Application Information

The TPS61240-Q1 boost regulator has fixed output voltage of 5 V typical with an input voltage range of 2.3 V to 5.5 V. TPS61240-Q1 allows the use of small inductors and capacitors to achieve a small solution size and supports output currents up to 450 mA. When shut down, the TPS61240-Q1 presents a high impedance at the VOUT pin and the load is disconnected completely from the battery. This allows for use in applications that require the regulated output bus to be driven by another supply while the TPS61240-Q1 is shut down.

Typical Applications

TPS61240-Q1 app_cir_lvsao4.gif Figure 9. TPS61240-Q1 Fixed 5 V Output from VIN = 3 V to 4.2 V

Design Requirements

Table 2 lists the design parameters for this application example.

Table 2. TPS61240-Q1 5V Output Design Requirements

PARAMETERS VALUE
Input voltage 3 V to 4.2 V
Output voltage 5 V
Output current 200 mA

Detailed Design Procedure

Programming the Output Voltage

The output voltage is set by an internal resistor divider. The FB pin is used to sense the output voltage. To configure the output properly, the FB pin has to be connected directly to the output.

Inductor Selection

For correct operation of TPS61240-Q1 device, an inductor must be connected between pin VIN and pin L. A boost converter requires two main passive components for storing energy during the conversion. A boost inductor and a storage capacitor at the output are required. To select the boost inductor, it is recommended to keep the possible peak inductor current below the current limit threshold of the power switch in the chosen configuration. The highest peak current through the inductor and the switch depends on the output load, the input (VIN), and the output voltage (VOUT). Estimation of the maximum average inductor current can be done using Equation 2.

Equation 2. TPS61240-Q1 eq2_il_max_lvsao4.gif

where

  • η is the efficiency of the switching regulator

For example, for an output current of 200 mA at 5 V VOUT, with efficiency of 85%, at least 392 mA of average current flows through the inductor at a minimum input voltage of 3 V.

The second parameter for choosing the inductor is the desired current ripple in the inductor. Normally, it is advisable to work with a ripple of less than 20% of the average inductor current. A smaller ripple (or larger inductor value) reduces the magnetic hysteresis losses in the inductor, as well as output voltage ripple and EMI. But with larger inductor, regulation time during load transients rises. In addition, a larger inductor increases the total system size and cost. With these parameters, it is possible to calculate the value of the minimum inductance by using Equation 3.

Equation 3. TPS61240-Q1 eq3_lmin_lvs806.gif

where

  • f is the switching frequency
  • ΔIL is the ripple current in the inductor

With VIN = 4.2 V, VOUT = 5 V, assuming inductor ripple current = 30% of minimum current limit of 0.5 A, the resulting inductor value = 1.28 μH. In typical applications, a 1.0 μH inductance is recommended. The device has been optimized to operate with inductance values between 1.0 μH and 2.2 μH. It is recommended that inductance values of at least 1.0 μH is used, even if Equation 3 yields something lower. Care has to be taken that load transients and losses in the circuit can lead to higher currents as estimated in Equation 3. Also, the losses in the inductor caused by magnetic hysteresis losses and copper losses are a major parameter for total circuit efficiency.

With the chosen inductance value, the peak current for the inductor in steady state operation can be calculated. Equation 4 shows how to calculate the peak current I.

Equation 4. TPS61240-Q1 eq4_il_peak_lvs806.gif

This would be the critical value for the current rating for selecting the inductor. It also needs to be taken into account that load transients and error conditions may cause higher inductor currents. Inductor with part number, LQM21PN1R0MC0 is one example of an inductor that can be used with this device. Customers need to verify and validate whether it is suitable for their application.

Input Capacitor

At least 2.2-μF input capacitor is recommended to improve transient behavior of the regulator and EMI behavior of the total power supply circuit. It is recommended to place a ceramic capacitor as close as possible to the VIN and GND pins

Output Capacitor

For the output capacitor, it is recommended to use small ceramic capacitors placed as close as possible to the VOUT and GND pins of the IC. If, for any reason, the application requires the use of large capacitors which can not be placed close to the IC, using a smaller ceramic capacitor in parallel to the large one is recommended. This small capacitor should be placed as close as possible to the VOUT and GND pins of the IC. To get an estimate of the recommended minimum output capacitance, Equation 5 can be used.

Equation 5. TPS61240-Q1 eq5_cmin_lvsao5.gif

where

  • ΔV is the maximum allowed ripple

With a chosen ripple voltage of 10 mV, a minimum effective capacitance of 2.3 μF is needed. The total ripple is larger due to the ESR of the output capacitor. This additional component of the ripple can be calculated using ΔVESR = IOUT × RESR

A capacitor with a value equal to or higher than the calculated minimum should be used. This is required to maintain control loop stability. There are no additional requirements regarding minimum ESR. There is no upper limit for the output capacitance value. Larger capacitors cause lower output voltage ripple as well as lower output voltage drop during load transients.

Note that ceramic capacitors have a DC bias effect, which will have a strong influence on the final effective capacitance. Therefore the correct capacitor value has to be chosen carefully. Package size and voltage rating in combination with material are responsible for differences between the rated capacitor value and the effective capacitance.

Checking Loop Stability

The first step of circuit and stability evaluation is to look from a steady-state perspective at the following signals:

  • Switching node, SW
  • Inductor current, IL
  • Output ripple voltage, VO(AC)

These are the basic signals that need to be measured when evaluating a switching converter. When the switching waveform shows large duty cycle jitter or the output voltage or inductor current shows oscillations, the regulation loop may be unstable. This is often a result of board layout and/or L-C combination.

As a next step in the evaluation of the regulation loop, the load transient response is tested. Time between the load transient and the turn on of the P-channel MOSFET, the output capacitor must supply all of the current required by the load. VO immediately shifts by an amount equal to ΔI(LOAD) × ESR, where ESR is the effective series resistance of CO. ΔI(LOAD) begins to charge or discharge CO generating a feedback error signal used by the regulator to return VO to its steady-state value. The results are very easily interpreted when the device operates in PWM mode. During recovery time, VO can be monitored for settling time, overshoot or ringing to judge the converter’s stability. Without any ringing, the loop has usually more than 45° of phase margin. Because the damping factor of the circuitry is directly related to several resistive parameters (for example, MOSFET rDS(on)) that are temperature dependant, the loop stability analysis has to be done over the input voltage range, load current range, and temperature range.

Application Curves

Table 3. Table of Application Curves

Figure
Waveforms Output voltage ripple, PFM mode, IOUT = 10 mA Figure 10
Output voltage ripple, PWM mode, IOUT = 150 mA Figure 11
Load transient response, VIN, 3.6 V, 0 mA to 50 mA Figure 12
Load transient response, VIN, 3.6 V, 50 mA to 200 mA Figure 13
Line transient response, VIN, 3.6 V to 4.2 V, IOUT = 50 mA Figure 14
Line transient response, VIN, 3.6 V to 4.2 V, IOUT = 200 mA Figure 15
Startup after enable, VIN, 3.6 V, VOUT = 5 V, Load = 5 kΩ Figure 16
Startup after enable, VIN, 3.6 V, VOUT = 5 V, Load = 16.5 kΩ Figure 17
Startup and shutdown, VIN, 3.6 V, VOUT = 5 V, Load = 16.5 kΩ Figure 18
TPS61240-Q1 pfm_ripple_lvs806.gif
Figure 10. Output Voltage Ripple – PFM Mode
TPS61240-Q1 load_trns_lvs806.gif
Figure 12. Load Transient Response
0 mA to 50 mA and 50 mA to 0 mA
TPS61240-Q1 line_trns_lvs806.gif
Figure 14. Line Transient Response
3.6 V to 4.2 V at 50 mA Load
TPS61240-Q1 start_no_load_lvs806.gif
Figure 16. Startup After Enable – No Load
TPS61240-Q1 stsh_w_load_lvs806.gif
Figure 18. Startup and Shutdown
TPS61240-Q1 pwm_ripple_lvs806.gif
Figure 11. Output Voltage Ripple – PWM Mode
TPS61240-Q1 load_trns3_lvs806.gif
Figure 13. Load Transient Response
0 mA to 200 mA and 200 mA to 0 mA
TPS61240-Q1 line_trns3_lvs806.gif
Figure 15. Line Transient Response
3.6 V to 4.2 V at 200 mA Load
TPS61240-Q1 start_w_load_lvs806.gif
Figure 17. Startup After Enable – With Load

System Example

Figure 19 is another example for using the TPS61240-Q1 with fixed 5 V and a Schottky diode for output overvoltage protection.

TPS61240-Q1 otg_app_lvsao4.gif Figure 19. TPS61240-Q1 Fixed 5 V With Schottky Diode for Output Overvoltage Protection