ZHCSFX6C March 2016 – May 2017 TAS5753MD
PRODUCTION DATA.
PIN | TYPE(1) | TERMINATION | DESCRIPTION | |
---|---|---|---|---|
NAME | NUMBER | |||
ADR/SPK_FAULT | 20 | DI/DO | — | Dual-function pin which sets the LSB of the 7-bit I2C address to 0 if pulled to GND, 1 if pulled to DVDD. If configured to be a fault output via the System Control Register 2 (0x05), the pin is pulled low when an internal fault with the speaker amplifier occurs. A pullup or pulldown resistor is required, as is shown in the . |
AGND | 36 | P | — | Ground for analog circuitry(3) |
AVDD | 19 | P | — | Power supply for internal analog circuitry |
ANA_REG1 | 18 | P | — | Linear voltage regulator output derived from AVDD supply which is used for internal analog circuitry. Nominal 1.8-V output.(2) |
ANA_REG2 | 37 | P | — | Linear voltage regulator output derived from AVDD supply which is used for internal analog circuitry. Nominal 3.3-V output.(2) |
BSTRPx | 3, 42, 46, 47 | P | — | Connection points for the bootstrap capacitors which are used to create a power supply for the high-side gate drive of the device. |
DGND | 35 | P | — | Ground for digital circuitry(3) |
DIG_REG | 24 | P | — | Linear voltage regulator output derived from the DVDD supply which is used for internal digital circuitry.(2) |
DR_CN | 12 | P | — | Negative pin for capacitor connection used in headphone amplifier and line driver charge pump |
DR_CP | 13 | P | — | Positive pin for capacitor connection used in headphone amplifier and line driver charge pump |
DR_INx | 7, 10 | AI | — | Input for channel A or B of headphone amplifier or line driver |
DR_OUTx | 8, 9 | AO | — | Output for channel A or B of headphone amplifier or line driver |
DR_SDI | 39 | DI | — | Places the headphone amplifier/line driver in shutdown when pulled low. |
DRVSS | 11 | P | — | Negative supply generated by charge pump for ground centered headphone and line driver output |
DRVDD | 14 | P | — | Power supply for internal headphone and line driver circuitry |
DVDD | 34 | P | — | Power supply for the internal digital circuitry |
GVDD_REG | 40 | P | — | Voltage regulator derived from PVDD supply(2) |
LRCLK | 26 | DI | Pulldown | Word select clock of the serial audio port. |
MCLK | 21 | DI | Pulldown | Master clock used for internal clock tree and sub-circuit and state machine clocking |
NC | 31 | — | — | Not connected inside the device (all NC terminals should be connected to ground for optimal thermal performance) |
OSC_GND | 23 | P | — | Ground for oscillator circuitry (the terminal should be connected to the system ground) |
OSC_RES | 22 | AO | — | Connection point for oscillator trim resistor |
PDN | 25 | DI | Pullup | Quick powerdown of the device that is used upon an unexpected loss of the PVDD or DVDD power supply to quickly transition the outputs of the speaker amplifier to Hi-Z. The quick powerdown feature avoids the audible anamolies that would occur as a result of loss of either of the supplies. |
PGND | 1, 44 | P | — | Ground for power device circuitry(3) |
PLL_FLTM | 16 | AI/AO | — | Negative connection point for the PLL loop filter components |
PLL_FLTP | 17 | AI/AO | — | Positive connection point for the PLL loop filter components |
PLL_GND | 15 | P | — | Ground for PLL circuitry (this terminal should be connected to the system ground) |
PowerPAD™ | — | P | — | Thermal and ground pad that provides both an electrical connection to the ground plane and a thermal path to the PCB for heat dissipation. The pad must be grounded to the system ground. (3) |
PVDD | 4, 41 | P | — | Power supply for internal power circuitry |
RST | 32 | DI | Pullup | Places the device in reset when pulled low |
SCL | 30 | DI | — | I2C serial control port clock |
SCLK | 27 | DI | Pulldown | Bit clock of the serial audio port |
SDA | 29 | DI/DO | — | I2C serial control port data |
SDIN | 28 | DI | Pulldown | Data line to the serial data port |
SPK_OUTx | 2, 43, 45, 48 | AO | — | Speaker amplifier outputs |
SSTIMER | 38 | AI | — | Controls ramp time of SPK_OUTx to minimize pop. Leave the pin floating for BD mode. Requires capacitor to GND in AD mode, as is shown in . The capacitor determines the ramp time. |
TEST1/TEST2 | 5/6 | DO | — | Used for testing during device production (the terminal must be left floating) |
TEST3 | 33 | DI | — | Used for testing during device production (the terminal must be connected to GND) |