ZHCSEC6B March 2012 – October 2015 LM3492HC , LM3492HC-Q1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The LM3429HC/-Q1 device is ideal for automotive and marine GPS display and applications that require a high contrast ratio.
The following procedures are to design an LED driver using the LM3492HC/-Q1 device.
The following procedures are to design an LED driver using the LM3492HC device with an input voltage ranged from 10 V to 24 V, and two LED strings consists of 10 LEDs each with a forward voltage of 3 V for each LED when running at 250 mA. The output power is 15 W. The switching frequency fSW is designed to be 300 kHz.
The nominal voltage of the LED string with 10 LEDs is 30 V, and the minimum voltage of the IOUTn pin (n = 1, 2) is 1.25 V when ILED is 250 mA. As a result, VOUT(nom) is 31.25 V. Design VOUT(max) to be 50 V. From Equation 5, VFB(nom) is approximately 1.8 V, which falls in the recommended operation range from 1.05 V to 2 V. Also, design RFB2 to be 16.2 kΩ. From Equation 3, RFB1 is calculated to be 265.1 kΩ, and a standard resistor value of 261 kΩ is selected. CFB is selected to be 10 pF as recommended.
The main parameter affected by the inductor is the peak to peak inductor current ripple (ILR). To maintain a continuous conduction mode (CCM) operation, ensure that the average inductor current IL1 is larger than half of ILR. For a boost converter, IL1 equals to the input current IIN. Hence,
Also,
If VIN is maximum, which is 24 V in this example, and only one LED string is turned on (because the two channels of the LM3492HC device are individually dimmable), IIN is minimum. From Equation 6 to Equation 8, it can be calculated that IIN(MIN), ton, and L1 are 0.326 A, 0.77 µs, and 28.5 µH. However,, from Equation 6, IIN is maximum when VIN is minimum, which is 10 V in this example, and the two LED strings are turned on together. Hence IIN(max) is 1.56 A. Then, ILR is
From Equation 7, ton is 2.27 µs. From (9), ILR is 0.80 A. The steady-state peak inductor current IL1(PEAK) is
As a result, IL1(PEAK) is 1.96 A. A standard value of 27 µH is selected for L1, and its saturation current is larger than 1.96 A.
The selection of the boost diode D1 depends on two factors. The first factor is the reverse voltage, which equals to VOUT for a boost converter. The second factor is the peak diode current at the steady state, which equals to the peak inductor current as shown in Equation 10. In this example, a 100-V 3-A schottky diode is selected.
The function of the input capacitor CIN and the output capacitor COUT is to reduce the input and output voltage ripples. Experimentation is usually necessary to determine their value. The rated DC voltage of capacitors used should be higher than the maximum DC voltage applied. Owing to the concern of product lifetime, TI recommends ceramic capacitors. But ceramic capacitors with high rated DC voltage and high capacitance are rare in general. Multiple capacitors connecting in parallel can be used for CIN and COUT. In this example, two 10-µF ceramic capacitor are used for CIN, and two 2.2-µF ceramic capacitor are used for COUT.
The capacitor on the VCC pin provides noise filtering and stabilizes the LDO regulator. It also prevents false triggering of the VCC UVLO. CVCC is recommended to be a 1-µF, good quality and low ESR ceramic capacitor.
The capacitor at the CDHC pin not only affects the sensitivity of the DHC but also determines the soft-start time tSS, the time for the output voltage to rise until power good. tSS is determined from the following equation:
In this example, CCDHC is recommended to be a 0.47-µF good quality and low ESR ceramic capacitor.
The resistors RRT and RIREF set the switching frequency fSW of the boost converter and the LED current ILED respectively. From Figure 19, if fSW is 300 kHz, RRT is selected to be 442 kΩ. From Figure 24, if ILED is 250 mA, RIREF is selected to be 4.99 kΩ.
Because the COMM pin is open drain, a resistor RCOMM of 52.3 kΩ is used to connect the VCC and COMM pins to act as a pullup function.
ILED = 150 mA | VOUT = 30 V | VVIN = 12 V | ||
Dimming frequency = 1 kHz | Trace 1 = VIOUT1 | Trace 4 = channel 1 LED |