In depth topic: Understanding Total Ionizing Dose (TID)
Learn about the impact of radiation on electronics in Space Applications. Cover the basics on Total Ionizing Dose.
00:19:07|24 6月 2016
The most common radiation requirement in the aerospace design community is Total Ionizing Dose (TID), also known as total dose. Total dose effects can lead to degradation and/or device failure. When a transistor can switch from a low-conductance (off) state to a high-conductance (on) state as the gate voltage passes through a threshold, it is operating properly. Hindrances to this functionality include extended exposure to TID radiation and an increase in the leakage current.
此视频是该系列的一部分
- T-60 视频系列 – 航天级电源管理电路的设计注意事项
(26 个视频)