EK-TM4C123GXL
Tiva™ C 系列 LaunchPad 评估套件
EK-TM4C123GXL
概述
TM4C123G LaunchPad 评估套件是一个低成本评估平台,适用于基于 Arm Cortex-M4 的微控制器。TM4C123GH6PM MCU 配备 80MHz Arm Cortex-M4F CPU、256kB 闪存和 32kB SRAM,为 USB 主机/器件/OTG 和两个 12 位 ADC 模块提供集成的 USB 2.0 支持。TM4C123GH6PM 还包括多个串行通信通道,例如 UART、SPI、I2C 和 CAN。TM4C123G LaunchPad 设计的亮点是 TM4C123GH6PM USB 2.0 器件接口以及休眠和 PWM 模块等其他器件功能。
EK-TM4C123GXL 具有用于自定义应用的可编程用户按钮和 RGB LED。可堆叠接头提供了连接 BoosterPack™ 插件模块的接口,可让您通过德州仪器 (TI) 的 BoosterPack 生态系统轻松扩展 TM4C123G LaunchPad 的功能。TI 开发的 TivaWare SDK 为 TM4C123G LaunchPad 提供所有外设的驱动程序以及数十个应用的示例代码。
特性
基于 ARM Cortex-M4F 的 MCU TM4C123GLaunchPad 评估套件 (EK-TM4C123GXL) 具有以下功能:
- 高性能 TM4C123GH6PM MCU:
- 80MHz 32 位基于 ARM Cortex-M4 的微控制器 CPU
- 256KB 闪存,256KB SRAM,2KB EEPROM
- 两个增强型控制器区域网 (CAN) 模块(需要 CAN 收发器)
- USB 2.0 主机/器件/OTG + PHY
- 两个 12 位 2MSPS ADC,运动控制 PWM
- 8 个 UART、6 个 I2C、4 个 SPI
- 板载电路内调试接口 (ICDI)
- USB Micro-B 型插头转 USB-A 型插头电缆
- 预置 RGB 快速启动应用
- 自述文档快速入门指南
随 TivaWare SDK 提供数十个应用示例
Arm Cortex-M4 MCU
立即订购并开发
EK-TM4C123GXL — Tiva™ C 系列 TM4C123G LaunchPad 评估套件
SW-EK-TM4C123GXL — 适用于 TM4C 系列的 TivaWare™ TM4C123G LaunchPad 评估板
EK-LM4F232GXL Kit Software
TivaWare for C Series 32-bit Windows Examples
硬件开发
文档
TivaWare for C Series Release Notes
TivaWare for C Series DriverLib User Guide
TivaWare for C Series USB Library User Guide
TivaWare for C Series Boot Loader User Guide
发布信息
Version: 2.0
Build date: 2013-08-29SW-TM4C — 适用于 C 系列的 TivaWare 软件(完整)
TivaWare for TM4C Series
EK-TM4C123GXL Kit Software
EK-TM4C1294XL Kit Software
EK-TM4C129EXL Kit Software
DK-TM4C129X Kit Software
TivaWare for TM4C Series Peripheral Driver Library
TivaWare for TM4C Series Graphics Library
TivaWare for TM4C Series Sensor Library
TivaWare for TM4C Series USB Library
TivaWare for C Series Windows Examples
产品
Arm Cortex-M4 MCU
硬件开发
文档
TivaWare for TM4C Series Peripheral Driver Library User Guide
TivaWare for TM4C Series Graphics Library User Guide
TivaWare for TM4C Series Sensor Library User Guide
TivaWare for TM4C Series USB Library User Guide
TivaWare for TM4C Series Boot Loader User Guide
TivaWare for TM4C Series Peripheral Examples User Guide
最新信息
The TivaWare™ Software Kit had been developed across a large number of years, originating from StellarisWare®. As a result of that, there were many elements that remained in TivaWare which were considerably out-of-date. In order to provide a cleaner user experience and better highlight relevant features for all customers, a lot of the outdated collateral has been removed.
This includes removing examples for evaluation kits that are no longer offered by Texas Instruments and outdated software libraries. A full list of removals can be found on the TivaWare Release Notes.
In addition, since the recommended evaluation kits for TM4C devices are the EK-TM4C123GXL and EK-TM4C1294XL LaunchPad™ development kits, new example projects have been added for both kits to provide a broader evaluation experience. For a full summary of bug fixes, changes, and improvements, view the latest TivaWare Release Notes.
发布信息
设计文件
技术文档
类型 | 标题 | 下载最新的英文版本 | 日期 | |||
---|---|---|---|---|---|---|
* | 数据表 | Tiva™ C Series TM4C123GH6PM Microcontroller Data Sheet 数据表 (Rev. E) | 2014年 6月 20日 | |||
* | 用户指南 | Tiva C Series TM4C123G LaunchPad Evaluation Kit User's Manual | 2013年 4月 15日 | |||
用户指南 | 用于 C 系列的 TivaWare™ 入门信息 (Rev. A) | PDF | HTML | 下载英文版本 (Rev.A) | PDF | HTML | 2022年 9月 21日 | |
应用手册 | 在 EK-TM4C123GXL LaunchPad 上使用 Edde Flex CAN 控制器 | PDF | HTML | 下载英文版本 | PDF | HTML | 2022年 4月 27日 | |
选择指南 | TM4C Microcontrollers (Rev. E) | 2020年 12月 9日 | ||||
用户指南 | TivaWare™ Peripheral Driver Library for C Series User's Guide (Rev. E) | 2020年 5月 14日 | ||||
应用手册 | Using USB Host Mode on the EK-TM4C123GXL LaunchPad | PDF | HTML | 2020年 5月 12日 | |||
证书 | EK-TM4C123GXL EC Declaration of Conformity (DoC) (Rev. A) | 2019年 1月 2日 | ||||
更多文献资料 | C2000™ TM4C12x Control + Automation MCUs | 2014年 6月 9日 | ||||
应用手册 | TM4C123x MCUs | 2013年 7月 31日 | ||||
白皮书 | An Introduction to the Tiva C Series Platform of Microcontrollers | 2013年 4月 12日 | ||||
更多文献资料 | Tiva C Series TM4C123G LaunchPad Evaluation Kit (Rev. A) | 2013年 4月 12日 |