选择版本
SIMPLELINK-CC32XX-SDK
SimpleLink™ Wi-Fi® CC32xx 软件开发套件 (SDK)
Link to Windows Installer for SimpleLink CC32XX SDK.
Link to macOS Installer for SimpleLink CC32XX SDK.
Link to Linux Installer for SimpleLink CC32XX SDK.
Link to Radio Tool for SimpleLink CC32XX SDK and SimpleLink SDK Wi-Fi Plug-In
产品
Wi-Fi 产品
硬件开发
文档
SimpleLink CC32XX SDK Documentation
发布信息
Click on the links in the table above to download. The SimpleLink Wi-Fi SDK delivers components that enable engineers to develop connected applications on Texas Instruments Wi-Fi micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
For CC3220 SDK versions 2.30 and earlier, please see the CC3220 SDK download page.
最新动态
- This is the initial SDK release with TI-RTOS7 examples. See note in Release Notes for more information.
- Updated FreeRTOS to version 202104.00
- OTA update – The Local and Cloud OTA have been removed from the SDK and are now obsolete, those examples could be evaluated in older SDKs if needed.A new OTA example with more advanced features will be added in an upcoming SDK.A preview of the new OTA example is linked in Release Notes
- Firmware bug fixes
- Please refer to the Documentation Overview for the details about each SDK component
- SimpleLink Platform level changes are available in SimpleLink Core SDK Release Notes
- SDK Change Log provides a list of all SDK component changes