选择版本
SIMPLELINK-CC32XX-SDK
SimpleLink™ Wi-Fi® CC32xx 软件开发套件 (SDK)
Link to Windows Installer for SimpleLink CC32XX SDK.
Link to macOS Installer for SimpleLink CC32XX SDK.
Link to macOS Installer for SimpleLink CC32XX SDK.
Link to Linux Installer for SimpleLink CC32XX SDK.
Link to Radio Tool for SimpleLink CC32XX SDK and SimpleLink SDK Wi-Fi Plug-In
产品
Wi-Fi 产品
硬件开发
文档
SimpleLink CC32XX SDK Documentation
发布信息
Click on the links in the table above to download. The SimpleLink Wi-Fi SDK delivers components that enable engineers to develop connected applications on Texas Instruments Wi-Fi micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
For CC3220 SDK versions 2.30 and earlier, please see the CC3220 SDK download page.
最新动态
- Support for WPA3 Personal in client mode. WPA3 introduces the use of Protected Management Frames (PMF) as well as using the Simultaneous Authentication of Equals (SAE) technique to authenticate clients instead of the Pre-shared Key (PSK) used in WPA2-Personal. See https://www.wi-fi.org/discover-wi-fi/security for more details on WPA3
- Added ability to disable legacy PS-Poll power save mechanism for improved compatibility with access points (APs), that do not fully support PS-Poll control frames. With PS-Poll disabled, the device still uses 802.11 power save mode, but will transition to active mode instead of using a PS-Poll frame to receive buffered unicast data from the AP