选择版本
SIMPLELINK-CC32XX-SDK
SimpleLink™ Wi-Fi® CC32xx 软件开发套件 (SDK)
Link to Windows Installer for SimpleLink CC32XX SDK. NOTE: CCS users must use CCS v9.2.0
Link to macOS Installer for SimpleLink CC32XX SDK. NOTE: CCS users must use CCS v9.2.0
Link to Linux Installer for SimpleLink CC32XX SDK. NOTE: CCS users must use CCS v9.2.0
Link to Radio Tool for SimpleLink CC32XX SDK and SimpleLink SDK Wi-Fi Plug-In
产品
Wi-Fi 产品
硬件开发
文档
SimpleLink CC32XX SDK Documentation
发布信息
Click on the links in the table above to download. The SimpleLink Wi-Fi SDK delivers components that enable engineers to develop connected applications on Texas Instruments Wi-Fi micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
For CC3220 SDK versions 2.30 and earlier, please see the CC3220 SDK download page.
最新动态
NOTE: CCS users must use CCS v9.2.0 or newer with this SDK
SIMPLELINK-CC32XX-SDK_3.30.01.02
- Added DICE unique Certificate Extensions to the Alias key certificate
- The DICE features requires SP 4.4.1.3_3.1.0.5_3.1.0.19.bin (provided with this SDK)
- Once version greater than 4.4.1.3 is used and the OTP section or DICE feature exists, the device cannot be downgraded to an older version of SP
SIMPLELINK-CC32XX-SDK_3.30.00.04
- Support for DICE - a security standard with hardware and software authentication using manufacturer servers based on the Microsoft Azure cloud service
- Documentation on how to use this feature can be found in Device Identity section in the UniFlash Users Guide
- NOTE: Enabling the DICE feature will be provided in the next release of the UniFlash
- Support RSA 4096bit keys for enterprise certificate validation
- CC3X20 - Support file signing with SHA-256 including mcu image file through OTA or SimpleLink host driver API - Uniflash is not supported
- Pass bonjour test version 1.5
- SDK examples configurable with sysconfig only
- SerialWifi demo application removed from the SDK
- Network terminal - Adding history to the CLI using up and down keys
- Ability to set pre-processed pre-master key instead of passphrase in WPA connection to an AP. This is done using new security type in the SimpleLink host driver 3.0.1.55
- Enable configuring GPIO 12 and 13 to work with the UART
- Various NWP bug fixes relating to HTTP and TCP retransmissions
- Various simplelink Wi-Fi host driver fixes relating to sync object handling
- Various OTA library fixes