选择版本

选择版本

未找到结果。请清除搜索并重试。

PROCESSOR-SDK-LINUX-OMAPL138

适用于 OMAP-L138 的 Linux 处理器 SDK

选择版本
未找到结果。请清除搜索并重试。

Code Composer Studio IDE for Windows Host

Code Composer Studio IDE for Linux Host

OMAPL138 Pin Mux Configuration Utility

Only used when creating an SD Card on Windows

SHA-256 校验和

OMAPL138 Linux SDK BSP Source Code

SHA-256 校验和

OMAPL138 Linux SDK prebuilt BSP binaries and root filesystem

SHA-256 校验和

OMAPL138 Linux SDK Arago source downloads

SHA-256 校验和
硬件开发
开发套件
TMDSLCDK138 OMAP-L138 开发套件 (LCDK)

文档

Instructions for creating an SD Card with Linux

Instructions for creating an SD Card with Windows

Link to Release Notes for Processor SDK Linux

Quick Start Guide included in the EVM kit (coming soon)

Link to the online Software Developers Guide which has the latest content

Software Manifest of Components Inside the SDK

发布信息

Thank you for your interest in the OMAPL138 Software Development Kit (SDK). This SDK supports the OMAPL138 Development KitTMDSLCDK138from TI. If you would like to install the full SDK on a Linux Host computer for development, you'll need the OMAPL138 Linux SDK Essentials below. If you would like to evaluate the SDK by running it on one of the below platforms and you prefer not to install the full SDK at this time, please see the OMAPL138 Linux SDK SD Card Creation section below.

More Information If you'd like more information on all of these choices, please refer to the Processor SDK Linux Getting Started Guide (GSG) below or the latest version here . For a complete overview of the SDK, please refer to the Processor SDK Linux Software Developer's Guide (SDG) below or the latest version here .